Other Parts Discussed in Thread: 4460
Hi,
I am using omap 4460 custom board with linux kernel 3.0.8 running on it. I am trying to up the nfc chip pn544 on the board. I integrated the pn544 driver in kernel. I am using i2c as host interface and got the follwing error when run the kernel:
NFC driver for PN544: pn544_init
[ 4.306701] NFC driver for PN544: Fast - No CRC check.
[ 4.312591]
[ 4.312622] Entered probe function -- NFC
[ 4.319030] pn544 3-0050: pn544_probe
[ 4.323242] pn544 3-0050: IRQ: 199
[ 4.327117]
[ 4.327117] <<<<<<<<<<<<<<<<<<<<<<<<<<----------------- Inside nfc_request_resources -- NFC ---------->>>>>>>>>>>>>>>>>>>
[ 4.341674]
[ 4.341705] <<<<<<<<<<<<<<<<<<<<<<<<<<----------------- Inside nfc_enable -- NFC
[ 4.351837] pn544 3-0050: now in HCI-mode
[ 4.372253] pn544: Got 6 at rset write:
[ 4.376464] 5
[ 4.378448] f9
[ 4.380584] 4
[ 4.382598] 0
[ 4.384582] c3
[ 4.386688] e5
[ 4.388824]
[ 4.403625] pn544 3-0050: send: -121
[ 4.419250] pn544 3-0050: send2: -121
[ 4.423370] pn544 3-0050: Write error to rset: -121
[ 4.428894]
[ 4.428924] Inside nfc_disable -- NFC
[ 4.434844] pn544 3-0050: Now in OFF-mode
[ 4.473937]
[ 4.473937] Inside nfc_free_resources -- NFC
[ 4.480651] pn544: probe of 3-0050 failed with error -121
Can any one tell what went wrong and why i2c write got failed.
Note:
[1] The pn544 driver code come along with the kernel is incomplete. There are no implementations for the platform dependent functions
struct pn544_nfc_platform_data {
int (*request_resources) (struct i2c_client *client);
void (*free_resources) (void);
void (*enable) (int fw);
int (*test) (void);
void (*disable) (void);
};
I am running these functions with the dummy functions.
Can any body tell me whether any kernel patch released with the implementations of the above functions.
Thanks in advance,
Kiran.