Dear Mr/Ms
We use C5504 - 150 MHz. According to SPRS659D Table 6.3 it should be used CLKIN for achivment 150 MHz. But our device includes other chip that requirs 32.768 kHz clock.
- Therefore DSP is started with pin CLK_SEL=0 and pin CLK_IN=0 and boot is performed. RTCCLKOUT is enabled.
- PLL is bypassed and reprogrammed to 150 MHz at CLKIN= 12 MHz
- External frequency 12 MHz is connected to CLKIN
- CLK_IN is switched to High.
- PLLBYPASS is disabled.
I have any questions:
- Is it possible the scenario above?
- Does RTCCLKOUT continue after switching to CLKIN or closed?
- May be used diferent frequency (not 12 MHz) as CLKIN in this scenario.
Thanks
Sergey Zevelev