This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

edma3 wait cycles

Hello,

I am using dma sample program located at   http://processors.wiki.ti.com/index.php/Programming_EDMA_without_EDMA3LLD_package

I have modified registers in this code for omap3 platform to use QDMA.

I want to dma 80 bytes from src to dst using 2D dma.

Here is snippet of the code.

----------------------------------------------------------------------------------------------------------------------------------------------------------------

SRC = (unsigned int)(srcBuff);

A_B_CNT = ((10 << 16u) | (8 & 0xFFFFu));    /* ACNT = 8, BCNT = 10 */

DST = (unsigned int)(dstBuff);

SRC_DST_BIDX = (32 << 16u) | (32 & 0xFFFFu);    /* SRC_BIDX = 32, DST_BIDX = 32 for example; since it is 2D to 2D transfer, DST_BIDX = stride set by user ,write to destination buffer in 2D  */

LINK_BCNTRLD = (1 << 16u) | 0xFFFFu;    /* LINK = 0xFFFF, BCNTRLD = 1 */

SRC_DST_CIDX = 0;

CCNT = 1;
 
/* Step 3: Triggering the Transfer and Waiting for Transfer Completion */
while(((IPR) & 0x1) == 0);

----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

When I measure dma completion cycles i.e dma wait cycles across while statement (above line) in CCSV5, cycles required to perform DMA are observed to be 1472 cycles.

When I modify code to transfer 4KB of data, cycles required are observed to be 7280 cycles.

I think these are very high numbers.

Are cycle numbers like this expected?

Thanks in advance.

Regards,

Mike