Other Parts Discussed in Thread: TVP7002
Hi all,
I am using ezsdk_5_03_01_15.
After running my capture-encode application for longer duration for 720P resolution, I randomly get following kernel crash.
VPSS_FVID2: queue timeout
kernel BUG at drivers/media/video/ti81xx/ti81xxvin_main.c:829!
Unable to handle kernel NULL pointer dereference at virtual address 00000000 pgd = d2c2c000
[00000000] *pgd=92cdc031, *pte=00000000, *ppte=00000000
Internal error: Oops: 817 [#1]
last sysfs file: /sys/power/state
Modules linked in: omaplfb pvrsrvkm ti81xxhdmi ti81xxvin tvp7002 ti81xxvo ti81xxfb vpss syslink
CPU: 0 Tainted: G W (2.6.37 #2)
PC is at __bug+0x20/0x2c
LR is at release_console_sem+0x198/0x1ac
pc : [<c0048dd8>] lr : [<c006cae0>] psr: 60000113
sp : c75a9b90 ip : c75a9ac8 fp : c75a9b9c
r10: 00000000 r9 : c75a9e08 r8 : c75a9e08
r7 : d0464504 r6 : cb63e880 r5 : d0464400 r4 : d2779800
r3 : 00000000 r2 : c04dd3f0 r1 : 00007447 r0 : 00000045
Flags: nZCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment user
Control: 10c5387d Table: 92c2c019 DAC: 00000015
Does any one know what is the root cause and fix for this issue ?
Regards,
Sweta