Other Parts Discussed in Thread: OMAP-L138, OMAPL138
We have a custom OMAP L-138 board with a revision 2.0 silicon chip.
The board doesn't boot reliably from power on. It prints some or all of
"OMAP-L138 initialization passed"
and dies. It works reliably from the reset button. We are working on the theory that it is caused by the Silicon Errata issue of requiring a double reset. If I understand the errata correctly, the ARM processor is never running. Hence my question:
Which processor (arm/dsp/?) prints the OMAP-L138 initialization passed" ?
If it's the ARM, I would think that counter indicates the lack of the double reset is a problem.
thanks in advance
tom campbell