This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CAN in DM6437



Hi.

I'm trying to send images processed in DM6437 by CAN bus at 500kbps. I use one PRD (periodic funcion) to send at least of 1 image/sec, with size of around 15kB. I have enough bandwith to trasfer this amount of data, but I realized that I need doing active waiting for send each CAN frame.I tested controller can't send more than 1 CAN frame each 250 us). For example if I do directly:

for (i=0 ;i<(IMAGE_SIZE/7) ;i++  )
    {
        if (numSec==257)
        {
            numSec=0;
        }
        tx_data_low = numSec<<24;
        numSec++;
        tx_data_high=0;

        for (j=0;j<7;j++)
        {
            if (j<3)
            {
                tx_data_low |= (0xFF & PICBMP[j+numFrames*7])<<(16-(j*8));
            }
            else
            {
                tx_data_high|= (0xFF & PICBMP[j+numFrames*7])<<(24-((j-3)*8));
            }
        }

        /* -------------------------------- *
         *  Transmit data async             *
         * -------------------------------- */
        
        can_tx_setup( mailboxSelected, msg_id_TX_2, DATA_LENGTH_8, PRIORITY_0 );
        can_tx( mailboxSelected, tx_data_low, tx_data_high );
        mailboxSelected++;
        if (mailboxSelected==3)
       {
            mailboxSelected=1;
       }
    }

where functions realated are:

/* ------------------------------------------------------------------------ *
 *  can_tx_setup( )                                                         *
 * ------------------------------------------------------------------------ */
Int16 can_tx_setup( Uint32 mailbox, Uint32 msg_id, Uint32 tx_length, Int32 tx_priority )
{
    Uint32 mailbox_bit = 1 << mailbox;

    tx_priority = tx_priority & 0x3F;
    tx_length   = tx_length & 0x0F;

    hecc->regs->ME &= ~mailbox_bit;             // Disable mailbox

    tx_msg_idreg = 0
        | ( STANDARD_ID << 31 )                 // Set the identifier type
        | ( 0 << 30 )                           // Clear Acceptance Mask Enable( AME )
        | ( 0 << 29 )                           // Auto-Answer mode( AAM )
        | ( msg_id << 0 );                      // Load the identifier

    tx_msg_mcfreg = 0
        | ( tx_priority << 8 )                  // Set Priority
        | ( 0 << 4 )                            // No Remote Frame
        | ( tx_length << 0 );                   // Data length

    hecc->regs->MD &= ~mailbox_bit;             // Set transmit mode
    hecc->regs->ME |= mailbox_bit;              // Enable mailbox

    hecc->regs->TA == 0;
    
    return 0;
}

/* ------------------------------------------------------------------------ *
 *  can_tx( )                                                               *
 * ------------------------------------------------------------------------ */
Int16 can_tx( Uint32 mailbox, Uint32 low, Uint32 high )
{
    Uint32 mailbox_bit = 1 << mailbox;

    /* Write into Mailbox# */
    hecc->regs->ME &= ~mailbox_bit;             // Disable MBX
    hecc->regs->MBX[mailbox].MID = tx_msg_idreg;
//   hecc->regs->ME |= mailbox_bit;              // Enable MBX
    hecc->regs->ME = mailbox_bit;              // Enable MBX

    hecc->regs->MBX[mailbox].MCF = tx_msg_mcfreg;
    hecc->regs->MBX[mailbox].MDL = low;
    hecc->regs->MBX[mailbox].MDH = high;
   
    /* Start transmission */
    hecc->regs->TRS |= mailbox_bit;
    while( hecc->regs->TA == 0 );

    return 0;
}

With that code, I lost some frame (it seems the controller is not quick enough and overwrite the mailboxes). TO resolve I need to put a delay of minimum of 250us.. in each iteration.

Could I increase this performance???

Thank a lot