Other Parts Discussed in Thread: OMAPL138, OMAP-L138
I'm trying to follow the instructions of the following wiki to program the SPI Flash connected to an OMAPL138 processor on a custom board. It freezes at at: "Waiting for SFT on the OMAP-L138..."
http://processors.wiki.ti.com/index.php/Boot_Images_for_OMAP-L138
We have the SPI Flash connected to SPI1 of the OMAPL138. The SPI flash we are using is the N25Q128A21.
Following is the output from the sfh utility (Perhaps it is also worth noting that I get something similar when I just try and erase the flash with the command: sfh_OMAP-L138.exe -erase -p COM5 -v):
D:\work\tmp\OMAP-L138_FlashAndBootUtils_2_40\OMAP-L138\GNU>sfh_OMAP-L138.exe -flash_noubl -p COM5 -v d:\work\tmp\ais.out
-----------------------------------------------------
TI Serial Flasher Host Program for OMAP-L138
(C) 2012, Texas Instruments, Inc.
Ver. 1.67
-----------------------------------------------------
[TYPE] Single boot image
[BOOT IMAGE] d:\work\tmp\ais.out
[TARGET] OMAPL138
[DEVICE] SPI_MEM
[SPI Block] 0
Attempting to connect to device COM5...
Press any key to end this program at any time.
(AIS Parse): Read magic word 0x41504954.
(AIS Parse): Waiting for BOOTME... (power on or reset target now)
(AIS Parse): BOOTME received!
(AIS Parse): Performing Start-Word Sync...
(AIS Parse): Performing Ping Opcode Sync...
(AIS Parse): Processing command 0: 0x58535901.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Loading section...
(AIS Parse): Loaded 9200-Byte section to address 0x80000000.
(AIS Parse): Processing command 1: 0x58535901.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Loading section...
(AIS Parse): Loaded 736-Byte section to address 0x800023F0.
(AIS Parse): Processing command 2: 0x58535906.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Performing jump and close...
(AIS Parse): AIS complete. Jump to address 0x80000000.
(AIS Parse): Waiting for DONE...
(AIS Parse): Boot completed successfully.
Waiting for SFT on the OMAP-L138...