Has anyone had luck using an external emulator to debug the AM3359 on either TMDXICE3359 (reworked to use 20pin CTI header) or TMDXIDK3359?
I am attempting to use the XDS510 USB from Spectrum Digital with CCSv5.
I had no trouble debugging with the XDS100v2 on the ICE board. Since converting the ICE to use the 20pin CTI I cannot load a program and debug. I changed the target configuration to use the XDS510 USB and I am able to connect to target and run the initizalization script. I performed the emulator test in SDCONFIG and 1 device was found in the JTAG chain. When I load a program I expect to stop at main, but the Debug window in CCSv5 indicates the program is already "Running" while I can see it is not.
I am having the same trouble debugging on the IDK.
Thank you.