Dear all,
I use DVRRDK to playback the audio through AIC3106 on DM8148EVM that the main chip uses PG2.1 and the EVM revision is C. But it sounds like trickplay, even if I set the sampling frequency to 8K or 16K. The consequence is all the same. If I set the
path of audio palyback to HDMI, the result is good. Can anyone guide me to modify this portion? Thanks in advance.
B.R.
OC