This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c6678 assembly



hello:

I write linear assembly, and --opt_level=2 ,  build  the assembly file,and generate .asm file,  I open the .asm file , find that  before PIPED LOOP PROLOG,  the compiler disable the  interrupt , and after PIPED LOOP EPILOG, compiler enable the  interrupt ,  I want to know if   when the assembly file is executed , a interrupt may be dropped! Because the interrupt is disable! So it may result some question! if so, what should I do?

if I do the SOFTWARE PIPELINE and do Optimization myself, need I disable the interrupt  before pipeline  loop,  enable the interrupt  after the pipeline  loop?????

thanks!

  • The interrupt will not be dropped, but it will not be taken during the execution of the short loop.  Basically, it cannot take an interrupt during the delay slots of a branch, doing so would result in the CorePac jumping back to wherever that branch was going to go.  So a short loop (i.e. 5 cycle or less) will prevent an interrupt from being taken while in the loop.  That said, the interrupt event still stays active and will be taken as soon as you leave the loop (i.e. as soon as you're not in the delay slots of a branch.)

    For more details please see chapter 6 of the C66x CPU and Instruction UG - SPRUGH7.

    Best Regards,
    Chad

  • hello:

     below is my assembly code,   Need I disable interrupt before loop kernel , and enable interrupt after loop kernel?

    thanks!
                                         .global _CplxMulCplx
    _CplxMulCplx:


    mv b6, b0 ;b0 = N
    || mv a4, a22 ;a22 = X = a0
    || mv a6, a23 ;a23 = Z = a3
    || mv b4, b22 ;b22 = Y
    mv b3, a14
    mv a6, b3
    || zero a1
    || zero b1
    shru b0, 2, b0 ;b0*2/8
    sub b0,2, b0 
    sub b0, 2, b0 

    lddw *b22++, a29:a28 ;a28 = pX[i+2], a29 = pX[i+3]
    lddw *a22++, a31:a30 ;a30 = pX[i] real; a31 = pX[i+1] imag

    lddw *a22++, b31:b30 ;b30 = pY[i] real; b31 = pY[i+1] imag
    lddw *b22++, b29:b28 ;b28 = pY[i+2], b29 = pY[i+3]

    lddw *b22++, a25:a24 ;a24 = pX[i+6], a25 = pX[i+7]
    lddw *a22++, a27:a26 ;a26 = pX[i+4], a27 = pX[i+5]

    lddw *a22++, b27:b26 ;b26 = pY[i+4], b27 = pY[i+5]
    || cmpysp a31:a30, a29:a28, a19:a18:a17:a16 ;1
    lddw *b22++, b25:b24 ;b24 = pY[i+6], b25 = pY[i+7]

    cmpysp b31:b30, b29:b28, b19:b18:b17:b16 ;2
    || lddw *b22++, a29:a28

    lddw *a22++, a31:a30

    cmpysp a27:a26, a25:a24, a7:a6:a5:a4 ;3
    || daddsp a19:a18, a17:a16, a21:a20 ;1
    || lddw *a22++, b31:b30

    lddw *b22++, b29:b28

    cmpysp b27:b26, b25:b24, b7:b6:b5:b4 ;4
    || daddsp b19:b18, b17:b16, b21:b20 ;2
    || lddw *b22++, a25:a24

    fsubsp b1, a21, b2 ;1
    || lddw *a22++, a27:a26

    daddsp a7:a6, a5:a4, a11:a10 ;3
    || mv a20, b9 ;1
    || lddw *a22++, b27:b26 ;b26 = pY[i+4], b27 = pY[i+5]
    || cmpysp a31:a30, a29:a28, a19:a18:a17:a16 ;1

    fsubsp a1, b21, a2 ;2
    || lddw *b22++, b25:b24

    ;loop kernel

    loop:
    daddsp b7:b6, b5:b4, b11:b10 ;4
    || mv b2, b8 ;1
    || mv b20, a13
    || cmpysp b31:b30, b29:b28, b19:b18:b17:b16 ;2
    || lddw *b22++, a29:a28

    stdw b9:b8, *b3++
    || fsubsp b1, a11, b2 ;3
    || addk 8, a23
    || lddw *a22++, a31:a30

    mv a2, a12 ;2
    || mv a10, b9
    || bdec loop,b0
    || cmpysp a27:a26, a25:a24, a7:a6:a5:a4 ;3
    || daddsp a19:a18, a17:a16, a21:a20 ;1
    || lddw *a22++, b31:b30

    stdw a13:a12, *a23++
    || fsubsp a1, b11, a2 ;4
    || addk 8, b3
    || lddw *b22++, b29:b28


    mv b2, b8 ;3
    || mv b10, a13
    || cmpysp b27:b26, b25:b24, b7:b6:b5:b4 ;4
    || daddsp b19:b18, b17:b16, b21:b20 ;2
    || lddw *b22++, a25:a24

    stdw b9:b8, *b3++
    || addk 8, a23
    || fsubsp b1, a21, b2 ;1
    || lddw *a22++, a27:a26

    mv a2, a12 ;4
    || daddsp a7:a6, a5:a4, a11:a10 ;3
    || mv a20, b9 ;1
    || lddw *a22++, b27:b26 ;b26 = pY[i+4], b27 = pY[i+5]
    || cmpysp a31:a30, a29:a28, a19:a18:a17:a16 ;1

    stdw a13:a12, *a23++
    || addk 8, b3
    || fsubsp a1, b21, a2 ;2
    || lddw *b22++, b25:b24


    ;LOOP EPILOG
    daddsp b7:b6, b5:b4, b11:b10 ;4
    || mv b2, b8 ;1
    || mv b20, a13
    || cmpysp b31:b30, b29:b28, b19:b18:b17:b16 ;2

    stdw b9:b8, *b3++
    || fsubsp b1, a11, b2 ;3
    || addk 8, a23

    mv a2, a12 ;2
    || mv a10, b9
    || cmpysp a27:a26, a25:a24, a7:a6:a5:a4 ;3
    || daddsp a19:a18, a17:a16, a21:a20 ;1

    stdw a13:a12, *a23++
    || fsubsp a1, b11, a2 ;4
    || addk 8, b3


    mv b2, b8 ;3
    || mv b10, a13
    || cmpysp b27:b26, b25:b24, b7:b6:b5:b4 ;4
    || daddsp b19:b18, b17:b16, b21:b20 ;2

    stdw b9:b8, *b3++
    || addk 8, a23
    || fsubsp b1, a21, b2 ;1

    mv a2, a12 ;4
    || daddsp a7:a6, a5:a4, a11:a10 ;3
    || mv a20, b9 ;1

    stdw a13:a12, *a23++
    || addk 8, b3
    || fsubsp a1, b21, a2 ;2

    daddsp b7:b6, b5:b4, b11:b10 ;4
    || mv b2, b8 ;1
    || mv b20, a13

    stdw b9:b8, *b3++
    || fsubsp b1, a11, b2 ;3
    || addk 8, a23

    mv a2, a12 ;2
    || mv a10, b9

    stdw a13:a12, *a23++
    || fsubsp a1, b11, a2 ;4
    || addk 8, b3

    mv b2, b8 ;3
    || mv b10, a13

    stdw b9:b8, *b3++
    || addk 8, a23

    mv a2, a12 ;4

    stdw a13:a12, *a23++
    || addk 8, b3

    ;结束
    mv a14, b3
    b b3
    nop 5

  • No, the only time you need to manually disable / enable interrupts is around ISR's.  This is done automatically if you use C to create your ISR's (interrupt service routines) and follow the instructions on how to create them.

    I believe you're confusing the fact that the HW will not let interrupts occur (with the exception of NMI and Reset) while in the delay slots of a branch and your need to disable and enable them.  As I've mentioned, you do not need to disable interrupts except for when creating an ISR, and again, if you simply use C to create your ISR using 'Interrupt' when declaring the ISR fuction, this is done automatically by the compiler.

    Best Regards,

    Chad

  • Hello Chad,

    You say that the interrupt will not be dropped, but it will be taken as soon as the loop execution is finished.

    Now, let us assume that the pipelined loop takes some time so that I receive another interrupt from the same source. Then what happens? Will the ISR connected to that interrupt be executed twice or just once? Does this situation differ wheteher the interrupt source is HW or SW, meaning HWI or SWI?

    Supposing that my ISR is executed only once, so this means that I missed the previous interrupt. Then what to do?

    Thank you,

    Abdulkerim

  • Chad Courtney said:

    No, the only time you need to manually disable / enable interrupts is around ISR's.  This is done automatically if you use C to create your ISR's (interrupt service routines) and follow the instructions on how to create them.

    This is like worst country song ever :-) "Around ISR"? "Done automatically if you use C to create your ISR's"? "Do not need to disable interrupts except for when creating an ISR"? No, no and no. If we talk about ISR, then if anything needs to be done about disabling/enabling interrupts, then it's specifically in ISR, not "around". ISR's are entered with interrupts disabled, but it has nothing to do with compiler. In fact C compiler is not in position to determine where or not interrupts can be enabled in ISR, ISR programmer is. As result compiler does exactly nothing about enabling/disabling interrupts in ISR, it's explicit programmer's responsibility. But as far as I can tell question is not about ISR at all...

    At the same time it should be noted that not all question are fair. One can not count on arbitrary, overly specific question to be directly answered. This is because specific aspects of specific code can be prohibitively hard to figure out. For example in this case question if interrupts need to be disabled can't be answered without deep understanding of algorithm and more importantly implementation itself. In extreme cases it might be easier for non-author to provide own implementation than to answer overly specific question about somebody else's one. What TI can and should do in such situation is to explain under which conditions interrupts would have to be disabled (yes,there are conditions even for plain, non-ISR code, after all, even compiler uses it occasionally, yes, even in non-ISR context), so that OP can judge whether or not it's the case for him-/herself. Yes, there are cases when interrupts are disabled implicitly (as correctly mentioned  for example in branch delay slots, SPLOOP is another example), but it doesn't change the principle that you have to recognize circumstances when they have to be disabled. Whether or not it happens implicitly or explicitly is implementation question, not principle.