This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

A problem of 6455 's pci

Hello, I have a pci care on wich the 6455 is the pci bridge. I pluged the card into a

computer's mainboard. The OS is WindowsXP. If  I send a host-to-dsp interrupt to Dsp by

DSPINT,  the host can't  recoganize  the PCI device and evne can't

read or write to the dsp pci memory AFTER REBOOT. It will lead to a OS crash.  But if I don't

send a host-to-dsp interrupt  and only do some memroy write and read to the dsp by  pci

memeroy map,it works very well  after reboot the host .
It seems that  if we send a host-to-dsp interrupt before host reboot, the dsp6455's PCI

config will go into an unknown state and the host can't read and write PCI bus

correctly after host reboot. I can only reset the dsp and then reboot the host again to

solve this problem. By the way, the 6455 is boot from ce3 's flash on this card.
SO  should I set other registers before the host reboot? Is it a bug of the 6455's pci

interface?

?