Hello Sitara Champs,
Do you have the ESD protection data on AM335x? We need both direct contact and indirect voltages.
Also do we have the EMI/EMC reports?
Kindly advise asap.
Best Regards,
Feroz
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Sitara Champs,
Do you have the ESD protection data on AM335x? We need both direct contact and indirect voltages.
Also do we have the EMI/EMC reports?
Kindly advise asap.
Best Regards,
Feroz
Hi Paul,
Thanks.
Our customer is asking for 6kV direct and 8kV indirect levels of protection.
Can this be mapped to the 3 metrics we have provided?
Human body model etc
Can you kindly clarify?
Thanks & Best Regards
Feroz
Hi Feroz,
HBM and CDM values are component-level ESD ratings. The ESD levels your customer is asking is system-level ESD ratings.
There is no clear correlation between two groups. I don't this TI device is designed to withstand direct system-level ESD stress (6 KV contact or 8 KV air).
What inferface/connector do they need 6 KV contact and 8 KV air on? They will probably need external board components to protect the IC against system-level ESD stress.
Best regards,
Jae