When I try to load the TMS320C6678 IBIS model downloaded from the TI website, I get the following error “Differential Pin N1 is paired with a NC pin."
The IBIS model is version 5.0, is there a newer version of the IBIS model?
As a workaround to verify the DDR III interface, we used the IBIS model from the C6670 to verify the DDR III interface. This helped us with this section of this board. We can not proceed further however. Is using the C6670 model acceptable for just this one interface?
Thanks,
Bryan Busacco