This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Sys/Bios examples give error

Every Sys/Bios example gives me "A device name must be specified". I followed the procedure. I am running CCSv4. Help, please.

 

  • Pat,

    Did you follow the BIOS_Getting_Started_Guide.pdf?

    I've attached it here for your convenience. 7827.Bios_Getting_Started_Guide.pdf

    Judah

  • Judah,

    Thanks for your response. I am using the V6.33 guide of Dec, 2011. I followed the procedure, but when I try to compile, it seems to think that I haven't selected a device for my platform, but I did select F28M35H52C1.

    Pat

     

  • Can you post the actual error here?

    Judah

  • Yes, here it is. Thanks for your response.

     

    **** Build of configuration Release for project sysbios7 ****

    C:\TI5\TI5_1\ccsv5\utils\bin\gmake -k all

    'Building file: ../hello.cfg'

    'Invoking: XDCtools'

    "C:/TI5/TI5_1/xdctools_3_22_04_46/xs" --xdcpath="C:/TI5/TI5_1/bios_6_32_05_54/packages;C:/TI5/TI5_1/ipc_1_23_05_40/packages;" xdc.tools.configuro -o configPkg -t ti.targets.arm.elf.M3 -p ti.platforms.concertoM3 -r release -c "C:/TI5/TI5_1/ccsv5/tools/compiler/tms470_4.9.5" "../hello.cfg"

    making package.mak (because of package.bld) ...

    generating interfaces for package configPkg (because package/package.xdc.inc is older than package.xdc) ...

    configuring hello.xem3 from package/cfg/hello_pem3.cfg ...

    error: ti.platforms.concertoM3.Platform: "C:/TI5/TI5_1/xdctools_3_22_04_46/packages/ti/platforms/concertoM3/Platform.xs", line 137: ti.platforms.concertoM3.Platform.Instance#0 : A device name must be specified for the platform 'ti.platforms.concertoM3'. A device name can be specified in the platform name, as 'ti.platforms.concertoM3:F28M35XXXXX', where F28M35XXXXX is the name of the selected device.

    js: "C:/TI5/TI5_1/xdctools_3_22_04_46/packages/xdc/cfg/Main.xs", line 149: Error: Configuration failed!

    gmake.exe: *** [package/cfg/hello_pem3.xdl] Error 1

    js: "C:/TI5/TI5_1/xdctools_3_22_04_46/packages/xdc/tools/Cmdr.xs", line 51: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.

    gmake: Target `all' not remade because of errors.

    **** Build Finished ****

  • Did you get through this problem?  Because I see that you are now having problems with the linker?

    If you did not, did you try what was suggested?  A device name can be specified in the platform name, as 'ti.platforms.concertoM3:F28M35XXXXX'

    Judah

  • Thanks, Judah. I have a solution to this problem. I thought I had already commented.

    Pat