This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 EZSDK booting output



Hi, all

I build the u-boot-2010.06-psp04.04.00.01 with command "make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm ti8168_evm_min_sd", that generated "u-boot.min.sd", I rename it to "MLO", then I compiled with command "make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm ti8168_evm_config_sd" that will generated "u-boot.bin", I copy both of them into the sd card(the boot partition), power up the 8168 EVM, but nothing output from uart2, what 's wrong?

Does "ti8168_evm_min_sd" suppress the console message as the  "ti8168_evm_config_quick_mmc"? how to enable uart message?