This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 EVM as PCIe endpoint



Hi,

I'm trying to operate DM8168 EVM in PCIe endpoint mode.

The Linux kernel I'm using comes from TI816X-LINUX-PSP-04.00.02.14.tgz.

I followed the instructions listed in http://processors.wiki.ti.com/index.php/DM81xx_AM38xx_PCI_Express_Endpoint_Driver_User_Guide

, disabled PCI bus support, and then enabled PCIE endpoint module.

I boot my EVM (single board, no connection to any PCIe root complex, just for test) with the new kernel image from SD card.

When I invoke insmod ti81xx_pcie_epdrv.ko command, it just returned an error message:

Unhandled fault: external abort on non-linefetch (0x1028) at 0xcb001004
Internal error: : 1028 [#1]
last sysfs file: /sys/kernel/uevent_seqnum
Modules linked in: ti81xx_pcie_epdrv(+)
CPU: 0    Not tainted  (2.6.37 #1)
PC is at ti81xx_ep_pcie_init+0x1b8/0x290 [ti81xx_pcie_epdrv]
LR is at kobject_put+0x48/0x5c
pc : [<bf000c1c>]    lr : [<c018e724>]    psr: 60000013
sp : c57cff18  ip : cb001050  fp : c57cff44
r10: 00000000  r9 : c57ce000  r8 : bf000e37
r7 : bf0011a8  r6 : 00000000  r5 : bf001198  r4 : cb000000
r3 : 00000000  r2 : cb001004  r1 : bf001210  r0 : bf001200
Flags: nZCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user
Control: 10c5387d  Table: 854a4019  DAC: 00000015
Process insmod (pid: 1152, stack limit = 0xc57ce2e8)
Stack: (0xc57cff18 to 0xc57d0000)
ff00:                                                       bf000e37 bf0011a8
ff20: c0085678 00000000 bf001074 00012008 00012018 bf000a64 c57cff7c c57cff48
ff40: c003942c bf000a70 bf001074 00012008 00012018 c0043fa8 00000000 bf001074
ff60: 00012008 00012018 c0043fa8 00000000 c57cffa4 c57cff80 c009574c c0039368
ff80: c00c0f64 c00c0e7c 00000000 00004000 00000003 00000080 00000000 c57cffa8
ffa0: c0043e00 c00956bc 00000000 00004000 00012018 00002d43 00012008 00000001
ffc0: 00000000 00004000 00000003 00000080 00012008 00000000 00012018 00000000
ffe0: bedbdead bedbdc3c 00008da0 401ae7d4 60000010 00012018 00000000 00000000
Backtrace:
[<bf000a64>] (ti81xx_ep_pcie_init+0x0/0x290 [ti81xx_pcie_epdrv]) from [<c003942c>] (do_one_initcall+0xd0/0x1a4)
 r8:bf000a64 r7:00012018 r6:00012008 r5:bf001074 r4:00000000
[<c003935c>] (do_one_initcall+0x0/0x1a4) from [<c009574c>] (sys_init_module+0x9c/0x1bc)
[<c00956b0>] (sys_init_module+0x0/0x1bc) from [<c0043e00>] (ret_fast_syscall+0x0/0x30)
 r7:00000080 r6:00000003 r5:00004000 r4:00000000
Code: e284cd41 e2822004 e584618c e28cc010 (e5923000)
---[ end trace baf535189e0c806b ]---

I traced into ti81xx_pcie_epdrv.c.

It hanged on line 851 in function ti81xx_setup_msi(), which reads control registers in the 0x51000000 region.

I wrote a program to read 0x51000000 via /dev/mem, It also causes a similar error message.

Unhandled fault: external abort on non-linefetch (0x1018) at 0x4038c000

Can anyone help?

  • I'm seeing a similar failure on a DM8148 EVM, with the kernel module included in the TI814X-LINUX-PSP-04.01.00.07 release.

    I'm also following the instructions on the wiki:  http://processors.wiki.ti.com/index.php/DM81xx_AM38xx_PCI_Express_Endpoint_Driver_User_Guide

    Has anyone successfully built and tested this module with a recent release?

    Can anyone @ TI verify that this should at least build and load out-of-the-box?

    Thanks.

    -Cory

    root@dm814x-evm:/opt/dvr_rdk/ti814x/kermod# insmod ./ti81xx_pcie_epdrv.ko
    Unhandled fault: external abort on non-linefetch (0x1028) at 0xcd001004
    Internal error: : 1028 [#1]
    last sysfs file: /sys/kernel/uevent_seqnum
    Modules linked in: ti81xx_pcie_epdrv(+)
    CPU: 0 Not tainted (2.6.37 #1)
    PC is at ti81xx_ep_pcie_init+0x1b8/0x290 [ti81xx_pcie_epdrv]
    LR is at kobject_put+0x48/0x5c
    pc : [<bf000c1c>] lr : [<c01ade44>] psr: 60000013
    sp : c36d7f18 ip : cd001050 fp : c36d7f44
    r10: 00000000 r9 : c36d6000 r8 : bf000e37
    r7 : bf0011a8 r6 : 00000000 r5 : bf001198 r4 : cd000000
    r3 : 00000000 r2 : cd001004 r1 : bf001210 r0 : bf001200
    Flags: nZCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment user
    Control: 10c5387d Table: 83460019 DAC: 00000015
    Process insmod (pid: 1122, stack limit = 0xc36d62e8)
    Stack: (0xc36d7f18 to 0xc36d8000)
    7f00: bf000e37 bf0011a8
    7f20: c0085638 00000000 bf001074 00012008 00012018 bf000a64 c36d7f7c c36d7f48
    7f40: c003942c bf000a70 bf001074 00012008 00012018 c0043fa8 00000000 bf001074
    7f60: 00012008 00012018 c0043fa8 00000000 c36d7fa4 c36d7f80 c0095930 c0039368
    7f80: c00c2428 c00c2340 00000000 00004000 00012018 00000080 00000000 c36d7fa8
    7fa0: c0043e00 c00958a0 00000000 00004000 00012018 00002d43 00012008 00000001
    7fc0: 00000000 00004000 00012018 00000080 00012008 00000000 00000003 00000000
    7fe0: bed3fec5 bed3fc5c 00008f5c 401bc7d4 60000010 00012018 00000000 00000000
    Backtrace:
    [<bf000a64>] (ti81xx_ep_pcie_init+0x0/0x290 [ti81xx_pcie_epdrv]) from [<c003942c>] (do_one_initcall+0xd0/0x1a4)
    r8:bf000a64 r7:00012018 r6:00012008 r5:bf001074 r4:00000000
    [<c003935c>] (do_one_initcall+0x0/0x1a4) from [<c0095930>] (sys_init_module+0x9c/0x1bc)
    [<c0095894>] (sys_init_module+0x0/0x1bc) from [<c0043e00>] (ret_fast_syscall+0x0/0x30)
    r7:00000080 r6:00012018 r5:00004000 r4:00000000
    Code: e284cd41 e2822004 e584618c e28cc010 (e5923000)
    ---[ end trace 8cb5e381e1be0009 ]---
    Segmentation fault
    root@dm814x-evm:/opt/dvr_rdk/ti814x/kermod#

  • Hello,

    As mentioned in the driver user guide, you need to follow the execution sequence extactly.

    In the first port, I see that SD boot mode is used, this means that the PCIe is not set in endpoint mode which EP driver expects.

  • I have the same problem with the first port,Is the endpoint must run in boot driver mode??

    Can anyone  help??

  • Hi Hemant:

    I want to use EP as non-pcie boot mode, should i have to add the

    EP initial sequences  rferred in TRM in the UBoot ?

    As i find that the ep uninitial at all, the reg 0x48140640 value is 0,

    no ep device is found at rc part.

    And i see no ep initial code to set PLL, mode , and so on,

    This should be done by ourself then?

    best regards

    xavier

  • Xavier said:
    I want to use EP as non-pcie boot mode, should i have to add the EP initial sequences  rferred in TRM in the UBoot ?

    That's what we did.  I believe newer U-Boot builds may already include some of the necessary setup (i.e. PCIe operating mode, PLL, etc.).  We don't actually map BARs, but we do set up the size and attributes - enough so that our host OS can enumerate the card as a PCI device and allocate appropriate resources.

  • Hi Cory:

    I find the pcie init code ,but it is ready for pcie_boot mode, in file

    ti_tools\linux_lsp\uboot\u-boot-dvr-rdk\arch\arm\cpu\arm_cortexa8\ti81xx\pcie.c

    whitout the moroc CONFIG_TI81XX_PCIE_BOOT and CONFIG_TI816X_MIN_CONFIG defined

    pcie_init will not be called,

    and if i enable this in \ti_tools\linux_lsp\uboot\u-boot-dvr-rdk\board\ti\ti8168\pcie.c

    this is pcie load ep mode, 

    not no-pcie load ep mode  what i really want ,

    so i try to dircect call this fun ,but it can not be complied for no pcie_init found even i 

    has include file #include <..\pcie.h>

    Code

    int misc_init_r (void)
    {
    #if defined(CONFIG_TI81XX_PCIE_BOOT) && defined(CONFIG_TI816X_MIN_CONFIG)
    extern int pcie_init(void);
    printf("\nSetting up for pcie boot...\n");
    pcie_init();
    return 0;
    #endif

    }

     

    int pcie_init(void)

    {
    int bar_enable_mask = 0;
    #ifndef TI81XX_NO_PIN_GPMC
    unsigned long long bar_size[6] = {0};
    #endif

    trig = 1;
    get_pcie_wdt_base_reload(&wdt_base, &wdt_reload);
    wdt_set_reload(wdt_base, wdt_reload);

    bootflag = (unsigned int) get_bootflag_addr();
    __raw_writel(0, bootflag);

    pcie_hw_setup();
    pcie_pll_setup();
    pcie_enable_module();
    app_retry_enable();
    DEBUGF("app_retry_enable() done\n");
    set_basic_config();
    DEBUGF("set basic config() done\n");

    write_pcie_lcfg_reg_bits(STATUS_COMMAND,
    CFG_REG_CMD_STATUS_MEM_SPACE_ENB,
    CFG_REG_CMD_STATUS_MEM_SPACE);
    enable_dbi_cs2();
    set_ti81xx_device_id();
    #ifdef CONFIG_TI81XX_PCIE_32
    #ifdef TI81XX_NO_PIN_GPMC
    set_size_config_32(&bar_enable_mask);
    #else
    get_size_boot_mode_pin_32(&bar_enable_mask, bar_size);
    set_size_pin_32(bar_size);
    #endif
    #endif

    #ifdef CONFIG_TI81XX_PCIE_64
    #ifdef TI81XX_NO_PIN_GPMC
    set_size_config_64(&bar_enable_mask);
    #else
    get_size_boot_mode_pin_64(&bar_enable_mask, bar_size);
    set_size_pin_64(bar_size);
    #endif
    #endif

    DEBUGF("set_bar_size() done\n");
    disable_dbi_cs2();
    DEBUGF("disable_dbi_cs2() done\n");
    #ifdef CONFIG_TI81XX_PCIE_32
    set_bar_config_32(&bar_enable_mask);
    #endif

    #ifdef CONFIG_TI81XX_PCIE_64
    set_bar_config_64(&bar_enable_mask);
    #endif

    DEBUGF("set_bar_config() done\n");
    config_appl_regs();
    DEBUGF("config_appl_regs() done\n");
    if (get_ti81xx_device_id() == TI8148_DEVICEID) {
    config_force_x1(); /* Not for TI816X */
    DEBUGF("config_force_x1() done\n");
    }
    pcie_enable_link();
    install_exceptions();
    wait_for_host();
    return 0;
    }

    best regards

    xavier

  • Xavier-

    We'd taken the U-Boot board support files (board/ti/ti8148/*), and "cloned" them to our own board type, allowing us a free hand to hack in exactly what was needed for our particular hardware and use cases.  I'm honestly not familiar with what (if any) magic combination of CONFIG_* macros will work with the default board support files to accomplish what you're trying to do.

    Below is just the applicable sequence of register writes we use for our hardware - this may prove a useful starting point if you head down a similar "custom board" path.  We simply call pcie_init() from s_init() following DDR setup every time.  Note also that we've tweaked the EP setup somewhat for our particular closed system - ours is a PCI card in a relatively "old", fixed, host system.  

    /* --- PCIe configuration functionality ------------------------------------- */
    
    static void pcie_hw_setup(void)
    {
        /* Set up Endpoint mode */
        __raw_writel(0x00000000, 0x48140480);  /* PCIE_CFG */
    }
    
    
    static void pcie_pll_setup(void)
    {
        __raw_writel(0x00000002, 0x48140E24);  /* SERDES_REFCLK_CTRL */
        delay(500);
    
        __raw_writel(0x00000000, 0x481406D8);  /* PCIE_PLLCFG0 */
        delay(500);
        __raw_writel(0x00640000, 0x481406DC);  /* PCIE_PLLCFG1 */
        delay(500);
        __raw_writel(0x00000000, 0x481406E0);  /* PCIE_PLLCFG2 */
        delay(500);
        __raw_writel(0x004008E0, 0x481406E4);  /* PCIE_PLLCFG3 */
        delay(500);
        __raw_writel(0x0000609C, 0x481406E8);  /* PCIE_PLLCFG4 */
        delay(500);
    
    #if 0
        /* WARNING!  WARNING!  WARNING!  WARNING!  WARNING!  WARNING!  WARNING!
         *
         * There is no reference to this particular register anywhere in either
         * the DM816x or DM814x technical literature.  In the original U-Boot
         * PCIe configuration, the corresponding write was commented out.
         *
         * For the time being, we'll leave it commented out and see what (if
         * anything) breaks.
         *
         * WARNING!  WARNING!  WARNING!  WARNING!  WARNING!  WARNING! WARNING!
         */
        __raw_writel(0x00000E7B, 0x48141318);  /* PCIE_SERDES_CFG_MISC */
        delay(500);
    #endif
    
        __raw_writel(0x00000004, 0x481406D8);  /* PCIE_PLLCFG0 */
        delay(500);
        __raw_writel(0x00000014, 0x481406D8);  /* PCIE_PLLCFG0 */
        delay(500);
        __raw_writel(0x00000016, 0x481406D8);  /* PCIE_PLLCFG0 */
        delay(500);
        __raw_writel(0x30000016, 0x481406D8);  /* PCIE_PLLCFG0 */
        delay(500);
        __raw_writel(0x70007016, 0x481406D8);  /* PCIE_PLLCFG0 */
        delay(2000);
        __raw_writel(0x70007017, 0x481406D8);  /* PCIE_PLLCFG0 */
    
        while ((__raw_readl(0x481406EC) & 0x00000001) == 0x00000000)
        {
            /* NOP */
        }
    }
    
    
    static void pcie_enable_module(void)
    {
        __raw_writel(0x0000009C, 0x48180B10);  /* RM_DEFAULT_RSTCTRL */
        delay(500);
    
        __raw_writel(0x00000000, 0x48180578);  /* CM_DEFAULT_PCI_CLKCTRL */
        __raw_writel(0x00000000, 0x48180510);  /* CM_DEFAULT_PCI_CLKSTCTRL */
        delay(500);
    
        __raw_writel(0x00000002, 0x48180510);  /* CM_DEFAULT_PCI_CLKSTCTRL */
        __raw_writel(0x00000002, 0x48180578);  /* CM_DEFAULT_PCI_CLKCTRL */
        delay(500);
    
        __raw_writel(0x0000001C, 0x48180B10);  /* RM_DEFAULT_RSTCTRL */
        delay(500);
    }
    
    
    static void pcie_setup_ep(void)
    {
        /* Set "Application Request Retry Enable" while we configure EP.
         * (CMD_STATUS) */
        __raw_writel(__raw_readl(0x51000004) | (1 << 4), 0x51000004);
    
        /* Set vendor & device ID. (VENDOR_DEVICE_ID) */
        __raw_writel(0x104C | (0xB801 << 16), 0x51001000);
    
        /* Enable device for memory accesses. (STATUS_COMMAND) */
        __raw_writel(__raw_readl(0x51001004) | (1 << 1), 0x51001004);
    
        /* Set CLASSCODE. (CLASSCODE_REVID) */
        __raw_writel(0x04000001, 0x51001008);
    
        /* Disable 64-bit MSI capability. */
        __raw_writel(__raw_readl(0x51001050) & ~(1 << 23), 0x51001050);
    
        /* Enable DBI_CS2 - allows BAR mask setup. (CMD_STATUS) */
        __raw_writel(__raw_readl(0x51000004) | (1 << 5), 0x51000004);
        while((__raw_readl(0x51000004) & (1 << 5)) == 0);
    
        /* Set BAR masks prior to enumeration by RC. */
        __raw_writel(0x00000FFF, 0x51001010);  /* BAR0: 4 KiB */
        __raw_writel(0x00007FFF, 0x51001014);  /* BAR1: 32 KiB */
        __raw_writel(0x00000000, 0x51001018);  /* BAR2: disabled */
        __raw_writel(0x00000000, 0x5100101C);  /* BAR3: disabled */
        __raw_writel(0x00000000, 0x51001020);  /* BAR4: disabled */
        __raw_writel(0x00000000, 0x51001024);  /* BAR5: disabled */
    
        /* Disable DBI_CS2. (CMD_STATUS) */
        __raw_writel(__raw_readl(0x51000004) & ~(1 << 5), 0x51000004);
    
        /* Set BAR access type and attributes after DBI_CS2 disable. */
        __raw_writel(0x00000000, 0x51001010);  /* BAR0: 32-bit, !pre-fetch */
        __raw_writel(0x00000000, 0x51001014);  /* BAR1: 32-bit, !pre-fetch */
        __raw_writel(0x00000000, 0x51001018);  /* BAR2: disabled */
        __raw_writel(0x00000000, 0x5100101C);  /* BAR3: disabled */
        __raw_writel(0x00000000, 0x51001020);  /* BAR4: disabled */
        __raw_writel(0x00000000, 0x51001024);  /* BAR5: disabled */
    
        /* Disable (skip over) exposing power management capabilities.
         *
         * Host system BIOS will place card into the D3 power state upon system
         * boot.  This results in the card not showing up in Windows - generally
         * considered a BadThing.  In order to avoid this unhappy state of affairs,
         * we're removing the PM capabilities entry from the extended configuration
         * section of the Local Configuration registers by pointing to the
         * descriptor immediately thereafter.
         */
        __raw_writel(0x00000050, 0x51001034);
    
        /* Enable [in/out]-bound address translation. (CMD_STATUS) */
        __raw_writel(__raw_readl(0x51000004) | (3 << 1), 0x51000004);
    
        /* Disable legacy (inbound), enable MSI (inbound), interrupts. */
        __raw_writel(0x0000000F, 0x5100018C);  /* IRQ_ENABLE_CLR */
        __raw_writel(0xFFFFFFFF, 0x51000108);  /* MSI0_IRQ_ENABLE_SET */
        __raw_writel(__raw_readl(0x51001050) | (1 << 16), 0x51001050);
    #if 0  /* Support for "Disable INTx" is PCI 2.3 or later. */
        __raw_writel(__raw_readl(0x51001004) | (1 << 10), 0x51001004);
    #endif
    
        /* Set x1 mode: LINK_CAP, PL_GEN2 & PL_LINK_CTRL */
        __raw_writel((__raw_readl(0x5100107C) & ~(0x3F <<  4)) | (1 <<  4), 0x5100107C);
        __raw_writel((__raw_readl(0x5100180C) & ~(0xFF <<  8)) | (1 <<  8), 0x5100180C);
        __raw_writel((__raw_readl(0x51001710) & ~(0x3F << 16)) | (1 << 16), 0x5100180C);
    }
    
    
    static void pcie_init(void)
    {
        pcie_hw_setup();
        pcie_pll_setup();
        pcie_enable_module();
        pcie_setup_ep();
    
        /* Enable LTSSM. (CMD_STATUS) */
        __raw_writel(__raw_readl(0x51000004) | 0x00000B01, 0x51000004);
        /* EP configuration done, disable app retry. (CMD_STATUS) */
        __raw_writel(__raw_readl(0x51000004) & ~(1 << 4), 0x51000004);
    }