This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to create no decoder VPFE with FVID_create() in DM6437 DSP/BIOS system?

Other Parts Discussed in Thread: TVP5146

Hi,

   I am trying to use FVID_create() config a no decoder VPFE  in DM6437 DSP/BIOS system.

   I find a deom for DM6437 EVM board : video_preview  in  C:\dvsdk_1_01_00_15\examples\video_preview.  

   In this project, tvp5146 as a decoder, convert the analog video signal to digital video signal.

   FVID_create()  FVID_control()  have been used to set config params for decoder and create a VPBE channel.  (code in the button)

   But I got a degital camera and no need a decoder in my system, based on the deom  project video_preview  ,how can i modify the project?

   I cry to use the project with no change,and the system out put a chaos color bar.

   I contast my system with the DM6437EVM board step by step, the problem may be on    FVID_dequeue(hGioVpfeCcdc, &frameBuffPtr);  

   After this code in evm board, "frameBuffPtr" point to "frameBuffTable[0]", in my system, "frameBuffPtr"  is always point to a wrong add such as 0xEBEBEBEB;

  who can give some suggestion? by the way ,in my system, the DSP I2C is not connected.



/* Set video display/capture driver params to defaults */
PSP_VPFE_TVP5146_ConfigParams tvp5146Params =
VID_PARAMS_TVP5146_DEFAULT;
PSP_VPFECcdcConfigParams vpfeCcdcConfigParams =
VID_PARAMS_CCDC_DEFAULT_D1;
PSP_VPBEOsdConfigParams vpbeOsdConfigParams =
VID_PARAMS_OSD_DEFAULT_D1;
PSP_VPBEVencConfigParams vpbeVencConfigParams;

standard = read_JP1();

/* Update display/capture params based on video standard (PAL/NTSC) */
if (standard == STANDARD_PAL) {
width = 720;
height = 576;
vpbeVencConfigParams.displayStandard = PSP_VPBE_DISPLAY_PAL_INTERLACED_COMPOSITE;
}
else {
width = 720;
height = 480;
vpbeVencConfigParams.displayStandard = PSP_VPBE_DISPLAY_NTSC_INTERLACED_COMPOSITE;
}
vpfeCcdcConfigParams.height = vpbeOsdConfigParams.height = height;
vpfeCcdcConfigParams.width = vpbeOsdConfigParams.width = width;
vpfeCcdcConfigParams.pitch = vpbeOsdConfigParams.pitch = width * 2;

/* init the frame buffer table */
for (i=0; i<FRAME_BUFF_CNT; i++) {
frameBuffTable[i] = NULL;
}

/* create video input channel */
if (status == 0) {
PSP_VPFEChannelParams vpfeChannelParams;
vpfeChannelParams.id = PSP_VPFE_CCDC;
vpfeChannelParams.params = (PSP_VPFECcdcConfigParams*)&vpfeCcdcConfigParams;
hGioVpfeCcdc = FVID_create("/VPFE0",IOM_INOUT,NULL,&vpfeChannelParams,NULL);
status = (hGioVpfeCcdc == NULL ? -1 : 0);
}

/* create video output channel, plane 0 */
if (status == 0) {
PSP_VPBEChannelParams vpbeChannelParams;
vpbeChannelParams.id = PSP_VPBE_VIDEO_0;
vpbeChannelParams.params = (PSP_VPBEOsdConfigParams*)&vpbeOsdConfigParams;
hGioVpbeVid0 = FVID_create("/VPBE0",IOM_INOUT,NULL,&vpbeChannelParams,NULL);
status = (hGioVpbeVid0 == NULL ? -1 : 0);
}

/* create video output channel, venc */
if (status == 0) {
PSP_VPBEChannelParams vpbeChannelParams;
vpbeChannelParams.id = PSP_VPBE_VENC;
vpbeChannelParams.params = (PSP_VPBEVencConfigParams *)&vpbeVencConfigParams;
hGioVpbeVenc = FVID_create("/VPBE0",IOM_INOUT,NULL,&vpbeChannelParams,NULL);
status = (hGioVpbeVenc == NULL ? -1 : 0);
}

/* configure the TVP5146 video decoder */
if (status == 0) {
result = FVID_control(hGioVpfeCcdc, VPFE_ExtVD_BASE+PSP_VPSS_EXT_VIDEO_DECODER_CONFIG, &tvp5146Params);
status = (result == IOM_COMPLETED ? 0 : -1);
}

/* allocate some frame buffers */
if (status == 0) {
for (i=0; i<FRAME_BUFF_CNT && status == 0; i++) {
result = FVID_allocBuffer(hGioVpfeCcdc, &frameBuffTable[i]);
status = (result == IOM_COMPLETED && frameBuffTable[i] != NULL ? 0 : -1);
}
}

/* prime up the video capture channel */
if (status == 0) {
FVID_queue(hGioVpfeCcdc, frameBuffTable[0]);
FVID_queue(hGioVpfeCcdc, frameBuffTable[1]);
FVID_queue(hGioVpfeCcdc, frameBuffTable[2]);
}

/* prime up the video display channel */
if (status == 0) {
FVID_queue(hGioVpbeVid0, frameBuffTable[3]);
FVID_queue(hGioVpbeVid0, frameBuffTable[4]);
FVID_queue(hGioVpbeVid0, frameBuffTable[5]);
}

/* grab first buffer from input queue */
if (status == 0) {
FVID_dequeue(hGioVpfeCcdc, &frameBuffPtr);
}

/* loop forever performing video capture and display */
while ( status == 0 ) {

/* grab a fresh video input frame */
FVID_exchange(hGioVpfeCcdc, &frameBuffPtr);

/* display the video frame */
FVID_exchange(hGioVpbeVid0, &frameBuffPtr);

}