Other Parts Discussed in Thread: TPS61325, SYSBIOS
Hi,
I am trying to enable camera in blaze tablet 2 which runs ICS 4A.1.4 release.I am using TEVM4XXX-CAM-V1-0 camera kit and connected it to Camera 1 (HDMI style) conector in the tablet.I opened the camera/cameraOMpa4 application in the tablet desktop.It is failing with error saying "Can't connect to the camera" error.
locat error message is as follows
V/CameraHolder( 671): open camera 0
E/CameraService( 128): CameraService::connect X (pid 671) rejected (invalid cameraId 0).
E/CameraHolder( 671): fail to connect Camera
E/CameraHolder( 671): java.lang.RuntimeException: Fail to connect to camera service
E/CameraHolder( 671): at android.hardware.Camera.native_setup(Native Method)
E/CameraHolder( 671): at android.hardware.Camera.<init>(Camera.java:302)
E/CameraHolder( 671): at android.hardware.Camera.open(Camera.java:264)
E/CameraHolder( 671): at com.ti.omap4.android.camera.CameraHolder.open(CameraHolder.java:131)
E/CameraHolder( 671): at com.ti.omap4.android.camera.Util.openCamera(Util.java:267)
E/CameraHolder( 671): at com.ti.omap4.android.camera.Camera$4.run(Camera.java:1487)
E/CameraHolder( 671): at java.lang.Thread.run(Thread.java:856)
D/OpenGLRenderer( 382): Flushing caches (mode 1)
D/dalvikvm( 190): GC_EXPLICIT freed 224K, 19% free 8736K/10759K, paused 2ms+3ms
D/OpenGLRenderer( 382): Flushing caches (mode 0)
V/camera ( 671): surfaceChanged. w=1003. h=752
I/Process ( 190): Sending signal. PID: 671 SIG: 3
I/dalvikvm( 671): threadid=3: reacting to signal 3
I/dalvikvm( 671): Wrote stack traces to '/data/anr/traces.txt'
I/ActivityManager( 190): Displayed com.ti.omap4.android.camera/.Camera: +603ms
W/ThrottleService( 190): unable to find stats for iface rmnet0
Please suggest.
Regards
Senthikumar R