Hello all,
If I may I would like to ask a question regarding connecting the console to UART2? If I config the GPIO_140,141,142 and 143 for the UART2
Would I be able to change the console from UART3 (presently) to UART2?
If I define the above GPIO’s as UART2 in mode 1 would the GPIO_144~147 would be available as UART2 in different mode as well. Basically we would have two uart2 AT THE SAME TIME.
Thanks for your reply in advance,
Ali.