I was using the TMS320C6454BZTZ7 and it is now NRND and looks I have to get the TMS320C6454BGTZA.
Are we going from lead free to leaded and then from commercial temp to industrial and also increasing the frequency to 850MHz? seems like an odd change and it's costing me $60 more - as I can no longer get my commercial 720MHz leaded device. Is there a PCN or some document describing the exact differences between the two devices?
Calum