Hello,
I have to obtain an one-seg brazilian compliant bitstream from a dm6467 encoder.
Comparing the dm6467 output with the one-seg standard, there are some mismatch.
- pic_order_cnt_type should be 2, but it is set to 0 from the encoder.
Is it enough to change this value in SPS and slice_header accordingly or something else must be done?
- constraint_setx_flag can be forced to the correct values?
Thanks
Claudio