This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

McBSP interrupt lines on Sitara AM398x

Hi all,

I'm having a problem to determine which interrupt line numbers are in use when I'm using McBSP interface, in my case for communication with audio codec.

As I can see from datasheet http://www.ti.com/lit/ds/sprs681d/sprs681d.pdf (page 150), McBSP has at least 3 interrupt lines (PORRINTERRUPT, PORXINTERRUPT, PORROVFLINTERRUPT) but when I start looking for where numbers in Cortex™-A8 Interrupt Controller Connections table there is only one interrupt for McBSP, int number 86.

I this some error in document and what are the real interrupt line numbers for McBSP interface? In driver code for McBSP I need to define which interrupt lines I'm using.

Best regards,

Srdjan