Other Parts Discussed in Thread: OMAP-L138, OMAP-L137
Hi,
My application requires sampling and real-time processing of 3 analog signals with maximum frequency of 1 MHz. I need to sample with atleast 2 MSPS ADC to avoid aliasing. After sampling each channel one by one, DSP will compute FFT and later on further post-processing over the FFT data will be performed. This system is intend to work stand alone.
I am precisely looking for;
1. High speed DSP to process 1 MHz signal in real-time.
2. DSP with atleast 3 Timer to signal 3 ADCs in parallel.
2. 3 or more channel ADC card- easy to interface with the chosen DSP.
3. 8192 or higher N point FFT computation.
4. Larger SDRAM to process large amount of data.
5. Larger Flash OR MMC/SD card feature to save larger amount of processed data to be further analyzed on Matlab or other software.
6. WLAN connectivity to send processed data to some storage unit.
I would really appreciate your help in selecting the right processor for my application.
Regards,
Tariq Siddiqui