This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

What is CSL function UART_write timeout units?

The TMS320C55x Chip Support Library API Reference Guide states:

Function CSLBool UART_write(char *pBuf, Uint16 length, Uint32 timeout);

Arguments

pbuf             Pointer to a data buffer
Length        Length of the data buffer
timeout       Time out for data ready.
                                 If it is setup as 0, means there will be no time out count.
                                 The function will block forever if THRE bit is not set.


However it doesn't say in what units is timeout? Is it in sec, milliseconds, microseconds, etc?

Thanks