Other Parts Discussed in Thread: OMAPL138, OMAP-L138, DA8XX, PMP
Hi,
Hoe can set OMAPL138 ethernet mac address to be fixed for all next boot ? [...because now the mac address change every boot? ]
During boot process i recieve this messages:
Booting TI User Boot Loader
UBL Version: 1.65
UBL Flashtype: SPI
Starting SPI Memory Copy...
Valid magicnum, 0x55424CBB, found at offset 0x00010000.
DONE
Jumping to entry point at 0xC1080000.
U-Boot 2009.11 (Jan 13 2011 - 01:05:37)
I2C: ready
DRAM: 64 MB
MMC: davinci: 0
In: serial
Out: serial
Err: serial
ARM Clock : 300000000 Hz
DDR Clock : 150000000 Hz
Invalid MAC address read.
Net: Ethernet PHY: GENERIC @ 0x00
Hit any key to stop autoboot: 0
reading uImage
2187060 bytes read
## Booting kernel from Legacy Image at c0700000 ...
Image Name: Arago/2.6.32+2.6.33-rc4-psp03.20
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2186996 Bytes = 2.1 MB
Load Address: c0008000
Entry Point: c0008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Linux version 2.6.33-rc4 (sdk@nemo) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #1 PREEMPT Thu Mar 24 23:27:57 CDT 2011
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
CPU: VIVT data cache, VIVT instruction cache
Machine: DaVinci DA850/OMAP-L138/AM18xx EVM
Memory policy: ECC disabled, Data cache writeback
DaVinci da850/omap-l138/am18xx variant 0x1
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 24320
Kernel command line: console=ttyS2,115200n8 noinitrd rw mem=32M@0xc0000000 mem=64M@0xc4000000 root=/dev/nfs nfsroot=10.0.0.26:/home/oded/DVSDK_4_02_00_06/OMAPL138/targetfs,nolock ip=dhcp
PID hash table entries: 512 (order: -1, 2048 bytes)
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 32MB 64MB = 96MB total
Memory: 92704KB available (4164K code, 320K data, 148K init, 0K highmem)
SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Hierarchical RCU implementation.
NR_IRQS:245
Console: colour dummy device 80x30
Calibrating delay loop... 149.50 BogoMIPS (lpj=747520)
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
DaVinci: 144 gpio irqs
regulator: core version 0.5
NET: Registered protocol family 16
da850_evm_init: mmcsd2 registration failed: -1bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
regulator: VDCDC1: 3200 <--> 3300 mV at 3300 mV
regulator: VDCDC2: 1750 <--> 3300 mV at 3300 mV
regulator: VDCDC3: 950 <--> 1375 mV at 1200 mV
regulator: LDO1: 1800 mV
regulator: LDO2: 1150 <--> 1300 mV at 1200 mV
pca953x 1-0020: failed reading register
i2c-gpio i2c-gpio.1: using pins 20 (SDA) and 21 (SCL)
Bluetooth: Core ver 2.15
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Switching to clocksource timer0_1
musb_hdrc: version 6.0, cppi4.1-dma, host, debug=0
Waiting for USB PHY clock good...
musb_hdrc: USB Host mode controller at fee00000 using DMA, IRQ 58
musb_hdrc musb_hdrc: MUSB HDRC host driver
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 3, 32768 bytes)
TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
EMAC: MII PHY configured, RMII PHY will not be functional
JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
msgmni has been set to 181
io scheduler noop registered (default)
da8xx_lcdc da8xx_lcdc.0: GLCD: Found Sharp_LK043T1DG01 panel
Console: switching to colour frame buffer device 60x34
Serial: 8250/16550 driver, 3 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO 0x1c42000 (irq = 25) is a AR7
serial8250.0: ttyS1 at MMIO 0x1d0c000 (irq = 53) is a AR7
serial8250.0: ttyS2 at MMIO 0x1d0d000 (irq = 61) is a AR7
console [ttyS2] enabled
brd: module loaded
ahci ahci: forcing PORTS_IMPL to 0x1
ahci ahci: AHCI 0001.0100 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
ahci ahci: flags: ncq sntf pm led clo only pmp pio slum part ccc
scsi0 : ahci
ata1: SATA max UDMA/133 irq 67
spi_davinci spi_davinci.1: DaVinci SPI driver in EDMA mode
Using RX channel = 18 , TX channel = 19 and event queue = 1
m25p80 spi1.0: m25p64 (8192 Kbytes)
Creating 4 MTD partitions on "m25p80":
0x000000000000-0x000000040000 : "U-Boot"
0x000000040000-0x000000050000 : "U-Boot Environment"
0x000000050000-0x0000007f0000 : "Linux"
0x0000007f0000-0x000000800000 : "MAC Address"
Read MAC addr from EEPROM: ff:ff:ff:ff:ff:ff
spi_davinci spi_davinci.1: Controller at 0xfef0e000
console [netcon0] enabled
netconsole: network logging started
ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
ohci ohci.0: DA8xx OHCI
ohci ohci.0: new USB bus registered, assigned bus number 2
ohci ohci.0: irq 59, io mem 0x01e25000
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
input: TPS6507x Touchscreen as /devices/platform/i2c-gpio.1/i2c-1/1-0048/input/input0
omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
omap_rtc: RTC power up reset detected
omap_rtc: already running
i2c /dev entries driver
Linux video capture interface: v2.00
usbcore: registered new interface driver uvcvideo
USB Video Class driver (v0.1.0)
watchdog watchdog: heartbeat 60 sec
Bluetooth: HCI UART driver ver 2.2
Bluetooth: HCI H4 protocol initialized
Bluetooth: HCI BCSP protocol initialized
Bluetooth: HCILL protocol initialized
cpuidle: using governor ladder
cpuidle: using governor menu
davinci_mmc davinci_mmc.0: Using DMA, 4-bit mode
davinci_mmc davinci_mmc.1: Using DMA, 4-bit mode
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
Advanced Linux Sound Architecture Driver Version 1.0.21.
usbcore: registered new interface driver snd-usb-audio
No device for DAI tlv320aic3x
asoc: tlv320aic3x <-> davinci-i2s mapping ok
ALSA device list:
#0: DA850/OMAP-L138 EVM (tlv320aic3x)
ata1: SATA link down (SStatus 0 SControl 300)
TCP cubic registered
NET: Registered protocol family 17
Bluetooth: L2CAP ver 2.14
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO (Voice Link) ver 0.6
Bluetooth: SCO socket layer initialized
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
Clocks: disable unused i2c1
Clocks: disable unused emac
Clocks: disable unused aemif
Clocks: disable unused spi0
Clocks: disable unused mcbsp0
Clocks: disable unused mcbsp1
Clocks: disable unused vpif
Clocks: disable unused ecap0
regulator_init_complete: incomplete constraints, leaving LDO2 on
regulator_init_complete: incomplete constraints, leaving LDO1 on
regulator_init_complete: incomplete constraints, leaving VDCDC3 on
regulator_init_complete: incomplete constraints, leaving VDCDC2 on
regulator_init_complete: incomplete constraints, leaving VDCDC1 on
davinci_emac_probe: using random MAC addr: 3a:1d:50:58:20:28
mmc0: new high speed SDHC card at address b368
mmcblk0: mmc0:b368 USD 3.75 GiB
mmcblk0: p1 p2
emac-mii: probed
omap_rtc omap_rtc: setting system clock to 2011-03-25 01:18:07 UTC (1301015887)
eth0: attached PHY driver [SMSC LAN8710/LAN8720] (mii_bus:phy_addr=1:00, id=7c0f1)
Sending DHCP requests .
PHY: 1:00 - Link is Up - 100/Full
., OK
IP-Config: Got DHCP answer from 0.0.0.0, my address is 10.0.0.62
IP-Config: Complete:
device=eth0, addr=10.0.0.62, mask=255.255.255.0, gw=10.0.0.138,
host=10.0.0.62, domain=, nis-domain=(none),
bootserver=0.0.0.0, rootserver=10.0.0.26, rootpath=
Looking up port of RPC 100003/2 on 10.0.0.26
Looking up port of RPC 100005/1 on 10.0.0.26
VFS: Mounted root (nfs filesystem) on device 0:13.
Freeing init memory: 148K
INIT: version 2.86 booting
Please wait: booting...
Starting udev
udev: starting version 141
udevd[564]: unable to move watches dir '/dev/.udev/watch', old watches will not be restored: Directory not empty
Remounting root file system...
FAT: bogus number of reserved sectors
VFS: Can't find a valid FAT filesystem on dev mmcblk0.
Caching udev devnodes
Populating dev cacheFAT: bogus number of reserved sectors
VFS: Can't find a valid FAT filesystem on dev mmcblk0p2.
mv: cannot rename '/tmp/devices': No such file or directory
NET: Registered protocol family 10
logger: mount: mount point /proc/bus/usb does not exist
ALSA: Restoring mixer settings...
NOT configuring network interfaces: / is an NFS mount
INIT: Entering runlevel: 5
Starting system message bus: dbus.
Starting Dropbear SSH server: dropbear.
Starting telnet daemon.
Starting syslogd/klogd: done
Starting thttpd.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org arago ttyS2
Arago 2011.02 arago ttyS2
arago login: root
root@arago:~#
Thanks, Oded.