Hi,
I am having problems with a VPSS M3 core crashing while creating a VFDC component or the associated control component. This is on the DM8168 EVM with EZSDK 5.04.00.11 and stock kernel/firmware/etc running our own userspace application talking to the M3 cores via OpenMAX.
The application creates and frees VFDC components several times (to reconfigure the output, since it doesn't offer any dynamic reconfiguration of layout or resolution), and at some point the OMX_GetHandle() call on either the VFDC or CTRL.DC components never returns (from the point of view of the A8). Looking at the logs via loggerSMDump shows a crash in the M3 firmware (see below).
The application is also doing some set of video operations using the M3 cores (video capture/encode/decode/scaling) which are hopefully irrelevant, but if any of that has some nasty interaction that I don't know about then do say and I can describe the relevant bits more carefully. The DSP is in use too, via C6Run.
Any ideas much appreciated,
- Mark
Here is the interesting bit of loggerSMDump output from one failing case (here dying when creating VPSSM3.CTRL.DC); other cases vary slightly, more log of this case and a different one (creating VPSSM3.VFDC) are attached. Note that the PC is the same in both cases.
N:VPSS P:2 #:04577 T:00000060cd0c8595 S:In OMX_GetHandle, component OMX.TI.VPSSM3.CTRL.DC, omxhandle 0x9f2a2f40
N:VPSS P:2 #:04578 T:00000060cd0d9131 S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<OMX_BASE_SetDefaultProperties> @line<1238>
N:VPSS P:2 #:04579 T:00000060cd0df72b S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<OMX_BASE_SetDefaultProperties> @line<1280> with error<0:ErrorNone>
N:VPSS P:2 #:04580 T:00000060cd0e91cf S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<OMX_BASE_ComponentInit> @line<133>
N:VPSS P:2 #:04581 T:00000060cd111b25 S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<_OMX_BASE_InitializePorts> @line<115>
N:VPSS P:2 #:04582 T:00000060cd11cc23 S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<_OMX_BASE_InitializePorts> @line<217> with error<0:ErrorNone>
N:VPSS P:2 #:04583 T:00000060cd17a8d5 S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<OMX_BASE_ComponentInit> @line<247> with error<0:ErrorNone>
N:VPSS P:2 #:04584 T:00000060cd1d3db7 S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<OMX_BASE_SetCallbacks> @line<267>
N:VPSS P:2 #:04585 T:00000060cd1da215 S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<OMX_BASE_SetCallbacks> @line<308> with error<0:ErrorNone>
N:VPSS P:2 #:04586 T:00000060cd1e068d S:Result of pComponentInit: ErrorNone
N:VPSS P:2 #:04587 T:00000060cd1e418d S:Registering the component OMX.TI.VPSSM3.CTRL.DC with TunnelMgr
N:VPSS P:2 #:04588 T:00000060cd1eacbb S:Entered: DomxTunnelMgr_registerHandle (0x9f2a2f40, 0x9f728654)
N:VPSS P:2 #:04589 T:00000060cd1f60af S:Entered function:OmxRpc_rcmClientCreate (0x9f29e2d0, OmxRpcRcmServer_OMX.TI.VPSSM3.CTRL.DC_Cb_3_18, 5)
N:VPSS P:2 #:04590 T:00000060cd1fd121 S:Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<983> msg<Before RcmClient_Params_init>
N:VPSS P:2 #:04591 T:00000060cd2034c2 S:Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<985> msg<After RcmClient_Params_init>
N:VPSS P:2 #:04592 T:00000060cd209203 S:Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<990> msg<Before RcmClient_create>
N:VPSS P:2 #:04593 T:00000060cd2adde3 S:Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<992> msg<After RcmClient_create>
N:VPSS P:2 #:04594 T:00000060cd2b6b73 S:main: calling RcmClient_getSymbolIndex(OmxRpcCbEventHandler)
N:VPSS P:2 #:04595 T:00000060cd4d091b S:main: calling RcmClient_getSymbolIndex(OmxRpcCbEmptyBufferDone)
N:VPSS P:2 #:04596 T:00000060cd4ff6d3 S:main: calling RcmClient_getSymbolIndex(OmxRpcCbFillBufferDone)
N:VPSS P:2 #:04597 T:00000060cd52c8db S:Module<ti.omx> @<domxtmgr_register_skelinfo> @line<417> msg<OmxRpcRcmServer_OMX.TI.VPSSM3.CTRL.DC_Ctrl_2_16>
N:VPSS P:2 #:04598 T:00000060cd536bbd S:OmxRpc_rcmIfGetHandle:ComponentName:OmxRpcRcmServer_OMX.TI.VPSSM3.CTRL.DC_Ctrl_2_16.Exiting..
N:VPSS P:2 #:04599 T:00000060cd9c9a59 S:FATAL ERROR: ErrorCode:0x1. Unhandled Exception:
N:VPSS P:2 #:04600 T:00000060cd9ce9ab S:Exception occurred in ThreadType_Task
N:VPSS P:2 #:04601 T:00000060cd9d232b S:handle: 0x9f277308.
N:VPSS P:2 #:04602 T:00000060cd9d5509 S:stack base: 0x9f277350.
N:VPSS P:2 #:04603 T:00000060cd9d897f S:stack size: 0x2000.
N:VPSS P:2 #:04604 T:00000060cd9dbbcd S:R0 = 0x9f2a9690 R8 = 0x9f167800
N:VPSS P:2 #:04605 T:00000060cd9dfa9f S:R1 = 0x00000001 R9 = 0x9f279640
N:VPSS P:2 #:04606 T:00000060cd9e37f1 S:R2 = 0x9f5b5021 R10 = 0x9f2a9824
N:VPSS P:2 #:04607 T:00000060cd9e76ab S:R3 = 0x9f583808 R11 = 0x9f27ea80
N:VPSS P:2 #:04608 T:00000060cd9eb50f S:R4 = 0x00028a84 R12 = 0x9f2a9bb8
N:VPSS P:2 #:04609 T:00000060cd9ef2cb S:R5 = 0x00000000 SP(R13) = 0x9f279110
N:VPSS P:2 #:04610 T:00000060cd9f3231 S:R6 = 0x9f167804 LR(R14) = 0x9f5c388d
N:VPSS P:2 #:04611 T:00000060cd9f723d S:R7 = 0x9f281a28 PC(R15) = 0x9f5b5090
N:VPSS P:2 #:04612 T:00000060cd9fb1d7 S:PSR = 0x41000000
N:VPSS P:2 #:04613 T:00000060cd9fe397 S:ICSR = 0x00400803
N:VPSS P:2 #:04614 T:00000060cda0164d S:MMFSR = 0x00
N:VPSS P:2 #:04615 T:00000060cda043ef S:BFSR = 0x82
N:VPSS P:2 #:04616 T:00000060cda070bd S:UFSR = 0x0000
N:VPSS P:2 #:04617 T:00000060cda09f05 S:HFSR = 0x40000000
N:VPSS P:2 #:04618 T:00000060cda0d0e5 S:DFSR = 0x00000000
N:VPSS P:2 #:04619 T:00000060cda1012f S:MMAR = 0x00028a84
N:VPSS P:2 #:04620 T:00000060cda13213 S:BFAR = 0x00028a84
N:VPSS P:2 #:04621 T:00000060cda16297 S:AFSR = 0x00000000
N:VPSS P:2 #:04622 T:00000060cda192e7 S:FATAL ERROR: ErrorCode:0x1. Terminating Execution...
Longer logs:
N:VPSS P:2 #:04409 T:00000060c46f2509 S:OmxRpc_rcmIfGetHandle:ComponentName:OMX.TI.VPSSM3.VFDC N:VPSS P:2 #:04410 T:00000060c46fc82f S:Entered function:omxrpc_module_init_client (3) N:VPSS P:2 #:04411 T:00000060c470123d S:LayerId: 2 N:VPSS P:2 #:04412 T:00000060c4709c21 S:@ omxrpc_rcm_server_create: rcmServerName OmxRpcRcmServer_OMX.TI.VPSSM3.VFDC_Ctrl_2_15, priority 14 N:VPSS P:2 #:04413 T:00000060c4710b27 S:Module<ti.omx> @<omxrpc_rcm_server_create> @line<225> msg<Before RcmServer_Params_init> N:VPSS P:2 #:04414 T:00000060c4716f11 S:Module<ti.omx> @<omxrpc_rcm_server_create> @line<229> msg<After RcmServer_Params_init> N:VPSS P:2 #:04415 T:00000060c471ce8b S:Module<ti.omx> @<omxrpc_rcm_server_create> @line<232> msg<Before RcmServer_create> N:VPSS P:2 #:04416 T:00000060c477d817 S:Module<ti.omx> @<omxrpc_rcm_server_create> @line<240> msg<After RcmServer_create> N:VPSS P:2 #:04417 T:00000060c47848bd S:@ omxrpc_rcm_server_remote_fxn_register regFxnCategory 1 N:VPSS P:2 #:04418 T:00000060c4789527 S:Calling RcmServer_addSymbol(OmxRpcSetParameter) N:VPSS P:2 #:04419 T:00000060c47917d1 S:Calling RcmServer_addSymbol(OmxRpcGetParameter) N:VPSS P:2 #:04420 T:00000060c4797305 S:Calling RcmServer_addSymbol(OmxRpcSetConfig) N:VPSS P:2 #:04421 T:00000060c479ed47 S:Calling RcmServer_addSymbol(OmxRpcGetConfig) N:VPSS P:2 #:04422 T:00000060c47a4589 S:Calling RcmServer_addSymbol(OmxRpcGetComponentVersion) N:VPSS P:2 #:04423 T:00000060c47aa341 S:Calling RcmServer_addSymbol(OmxRpcGetExtensionIndex) N:VPSS P:2 #:04424 T:00000060c47aff85 S:Calling RcmServer_addSymbol(OmxRpcGetState) N:VPSS P:2 #:04425 T:00000060c47b53d8 S:Calling RcmServer_addSymbol(OmxRpcSendCommand) N:VPSS P:2 #:04426 T:00000060c47bae05 S:Calling RcmServer_addSymbol(OmxRpcUseBuffer) N:VPSS P:2 #:04427 T:00000060c47c0585 S:Calling RcmServer_addSymbol(OmxRpcAllocBuffer) N:VPSS P:2 #:04428 T:00000060c47c5f75 S:Calling RcmServer_addSymbol(OmxRpcFreeBuffer) N:VPSS P:2 #:04429 T:00000060c47cb926 S:Calling RcmServer_addSymbol(OmxRpcEmptyThisBuffer) N:VPSS P:2 #:04430 T:00000060c47d12ed S:Calling RcmServer_addSymbol(OmxRpcFillThisBuffer) N:VPSS P:2 #:04431 T:00000060c47d7755 S:Calling RcmServer_addSymbol(OmxRpcTunnelRequest) N:VPSS P:2 #:04432 T:00000060c47ddc93 S:Module<ti.omx> @<omxrpc_rcm_server_start> @line<256> msg<Before RcmServer_start> N:VPSS P:2 #:04433 T:00000060c47e79af S:Module<ti.omx> @<omxrpc_rcm_server_start> @line<258> msg<After RcmServer_start> N:VPSS P:2 #:04434 T:00000060c47edd83 S:Instance Register with omxRpc Module.Cnt = 4 N:VPSS P:2 #:04435 T:00000060c47f1ac9 S:L_create: OmxRpc create: Component:OMX.TI.VPSSM3.VFDC, Layer:2 N:VPSS P:2 #:04436 T:00000060c47f765d S:Component OMX.TI.VPSSM3.VFDC In table OMX.TI.VPSSM3.VFCC idx 0 N:VPSS P:2 #:04437 T:00000060c47fc6f9 S:Component OMX.TI.VPSSM3.VFDC In table OMX.TI.VPSSM3.VFDC idx 1 N:VPSS P:2 #:04438 T:00000060c4801563 S:Component OMX.TI.VPSSM3.VFDC found idx: 1 N:VPSS P:2 #:04439 T:00000060c4806eed S:In OMX_GetHandle, component OMX.TI.VPSSM3.VFDC, omxhandle 0x9f225750 N:VPSS P:2 #:04440 T:00000060c485a411 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_SetDefaultProperties> @line<1238> N:VPSS P:2 #:04441 T:00000060c4862bd0 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_SetDefaultProperties> @line<1280> with error<0:ErrorNone> N:VPSS P:2 #:04442 T:00000060c48699d5 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_ComponentInit> @line<133> N:VPSS P:2 #:04443 T:00000060c4887db1 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_InitializePorts> @line<115> N:VPSS P:2 #:04444 T:00000060c4960973 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_InitializePorts> @line<217> with error<0:ErrorNone> N:VPSS P:2 #:04445 T:00000060c4ab6f97 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_ComponentInit> @line<247> with error<0:ErrorNone> N:VPSS P:2 #:04446 T:00000060c4ac4577 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:04447 T:00000060c4ac9e23 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:04448 T:00000060c4ad092d S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:04449 T:00000060c4ad7545 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:04450 T:00000060c4ade249 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:04451 T:00000060c4ae317d S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:04452 T:00000060c4ae954d S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:04453 T:00000060c4af0061 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:04454 T:00000060c4af8e91 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:04455 T:00000060c4afdf27 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:04456 T:00000060c4b04411 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:04457 T:00000060c4b0af75 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:04458 T:00000060c4b11b27 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:04459 T:00000060c4b16a63 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:04460 T:00000060c4b1cd5d S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:04461 T:00000060c4b23871 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:04462 T:00000060c4b2a557 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:04463 T:00000060c4b2f7d3 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:04464 T:00000060c4b35ccd S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:04465 T:00000060c4b3c7b9 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:04466 T:00000060c4b4356f S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:04467 T:00000060c4b484cf S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:04468 T:00000060c4b4e7c7 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:04469 T:00000060c4b55385 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:04470 T:00000060c4b5bdf5 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:04471 T:00000060c4b60d3f S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:04472 T:00000060c4b67041 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:04473 T:00000060c4b6f4d7 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:04474 T:00000060c4b762f9 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:04475 T:00000060c4b7b28d S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:04476 T:00000060c4b816c1 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:04477 T:00000060c4b881e5 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:04478 T:00000060c4b8ed4d S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:04479 T:00000060c4b93cbd S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:04480 T:00000060c4b99fd3 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:04481 T:00000060c4ba0b0b S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:04482 T:00000060c4ba7ba3 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:04483 T:00000060c4bacb01 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:04484 T:00000060c4bb2f71 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:04485 T:00000060c4bb9aed S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:04486 T:00000060c4bc05c7 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:04487 T:00000060c4bc55a5 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:04488 T:00000060c4bcb999 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:04489 T:00000060c4bd24cd S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:04490 T:00000060c4bd901f S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:04491 T:00000060c4bddf9d S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:04492 T:00000060c4be42db S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:04493 T:00000060c4bec8eb S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:04494 T:00000060c4bf395d S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:04495 T:00000060c4bf88cd S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:04496 T:00000060c4bfed53 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:04497 T:00000060c4c0585d S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:04498 T:00000060c4c0c455 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:04499 T:00000060c4c113af S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:04500 T:00000060c4c176d9 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:04501 T:00000060c4c1e403 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:04502 T:00000060c4c255ad S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:04503 T:00000060c4c2a6d9 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:04504 T:00000060c4c30aa3 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:04505 T:00000060c4c376a9 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:04506 T:00000060c4c3e269 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:04507 T:00000060c4c432b3 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:04508 T:00000060c4c495fb S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:04509 T:00000060c4c5023f S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:04510 T:00000060c4c56e11 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:04511 T:00000060c4c5bdf1 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:04512 T:00000060c4c63c19 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:04513 T:00000060c4c6abaf S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:04514 T:00000060c4c71a0d S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:04515 T:00000060c4c76a07 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:04516 T:00000060c4c7cda5 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:04517 T:00000060c4c8388f S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:04518 T:00000060c4c8a42f S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:04519 T:00000060c4c8f3cb S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:04520 T:00000060c4c9574b S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:04521 T:00000060c4c9c631 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:04522 T:00000060c4ca369b S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:04523 T:00000060c4ca8687 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:04524 T:00000060c4cae9b9 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:04525 T:00000060c4cb568b S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:04526 T:00000060c4cbc877 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_SetCallbacks> @line<267> N:VPSS P:2 #:04527 T:00000060c4cc34a1 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_SetCallbacks> @line<308> with error<0:ErrorNone> N:VPSS P:2 #:04528 T:00000060c4ccb177 S:Result of pComponentInit: ErrorNone N:VPSS P:2 #:04529 T:00000060c4ccf4fb S:Registering the component OMX.TI.VPSSM3.VFDC with TunnelMgr N:VPSS P:2 #:04530 T:00000060c4cd424f S:Entered: DomxTunnelMgr_registerHandle (0x9f225750, 0x9f727d54) N:VPSS P:2 #:04531 T:00000060c4ce211b S:Entered function:OmxRpc_rcmClientCreate (0x9f220b40, OmxRpcRcmServer_OMX.TI.VPSSM3.VFDC_Cb_3_17, 5) N:VPSS P:2 #:04532 T:00000060c4ce99e3 S:Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<983> msg<Before RcmClient_Params_init> N:VPSS P:2 #:04533 T:00000060c4cf11a1 S:Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<985> msg<After RcmClient_Params_init> N:VPSS P:2 #:04534 T:00000060c4cf8c47 S:Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<990> msg<Before RcmClient_create> N:VPSS P:2 #:04535 T:00000060c4d7c347 S:Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<992> msg<After RcmClient_create> N:VPSS P:2 #:04536 T:00000060c4d84af9 S:main: calling RcmClient_getSymbolIndex(OmxRpcCbEventHandler) N:VPSS P:2 #:04537 T:00000060c4db3bd7 S:main: calling RcmClient_getSymbolIndex(OmxRpcCbEmptyBufferDone) N:VPSS P:2 #:04538 T:00000060c4ddf4eb S:main: calling RcmClient_getSymbolIndex(OmxRpcCbFillBufferDone) N:VPSS P:2 #:04539 T:00000060c4e1cb93 S:Module<ti.omx> @<domxtmgr_register_skelinfo> @line<417> msg<OmxRpcRcmServer_OMX.TI.VPSSM3.VFDC_Ctrl_2_15> N:VPSS P:2 #:04540 T:00000060c4e26beb S:OmxRpc_rcmIfGetHandle:ComponentName:OmxRpcRcmServer_OMX.TI.VPSSM3.VFDC_Ctrl_2_15.Exiting.. N:VPSS P:2 #:04541 T:00000060ccf50a6b S:OmxRpc_rcmIfGetHandle:ComponentName:OMX.TI.VPSSM3.CTRL.DC N:VPSS P:2 #:04542 T:00000060ccf5b365 S:Entered function:omxrpc_module_init_client (3) N:VPSS P:2 #:04543 T:00000060ccf5ffc3 S:LayerId: 2 N:VPSS P:2 #:04544 T:00000060ccf68d05 S:@ omxrpc_rcm_server_create: rcmServerName OmxRpcRcmServer_OMX.TI.VPSSM3.CTRL.DC_Ctrl_2_16, priority 14 N:VPSS P:2 #:04545 T:00000060ccf6f739 S:Module<ti.omx> @<omxrpc_rcm_server_create> @line<225> msg<Before RcmServer_Params_init> N:VPSS P:2 #:04546 T:00000060ccf75ab1 S:Module<ti.omx> @<omxrpc_rcm_server_create> @line<229> msg<After RcmServer_Params_init> N:VPSS P:2 #:04547 T:00000060ccf7babd S:Module<ti.omx> @<omxrpc_rcm_server_create> @line<232> msg<Before RcmServer_create> N:VPSS P:2 #:04548 T:00000060cd00dc9b S:Module<ti.omx> @<omxrpc_rcm_server_create> @line<240> msg<After RcmServer_create> N:VPSS P:2 #:04549 T:00000060cd016a13 S:@ omxrpc_rcm_server_remote_fxn_register regFxnCategory 1 N:VPSS P:2 #:04550 T:00000060cd01bc6d S:Calling RcmServer_addSymbol(OmxRpcSetParameter) N:VPSS P:2 #:04551 T:00000060cd025433 S:Calling RcmServer_addSymbol(OmxRpcGetParameter) N:VPSS P:2 #:04552 T:00000060cd02b167 S:Calling RcmServer_addSymbol(OmxRpcSetConfig) N:VPSS P:2 #:04553 T:00000060cd0306cd S:Calling RcmServer_addSymbol(OmxRpcGetConfig) N:VPSS P:2 #:04554 T:00000060cd03616b S:Calling RcmServer_addSymbol(OmxRpcGetComponentVersion) N:VPSS P:2 #:04555 T:00000060cd03c059 S:Calling RcmServer_addSymbol(OmxRpcGetExtensionIndex) N:VPSS P:2 #:04556 T:00000060cd041b15 S:Calling RcmServer_addSymbol(OmxRpcGetState) N:VPSS P:2 #:04557 T:00000060cd047149 S:Calling RcmServer_addSymbol(OmxRpcSendCommand) N:VPSS P:2 #:04558 T:00000060cd04e157 S:Calling RcmServer_addSymbol(OmxRpcUseBuffer) N:VPSS P:2 #:04559 T:00000060cd056023 S:Calling RcmServer_addSymbol(OmxRpcAllocBuffer) N:VPSS P:2 #:04560 T:00000060cd05d30d S:Calling RcmServer_addSymbol(OmxRpcFreeBuffer) N:VPSS P:2 #:04561 T:00000060cd064ef1 S:Calling RcmServer_addSymbol(OmxRpcEmptyThisBuffer) N:VPSS P:2 #:04562 T:00000060cd06bd45 S:Calling RcmServer_addSymbol(OmxRpcFillThisBuffer) N:VPSS P:2 #:04563 T:00000060cd0717e1 S:Calling RcmServer_addSymbol(OmxRpcTunnelRequest) N:VPSS P:2 #:04564 T:00000060cd07b269 S:Module<ti.omx> @<omxrpc_rcm_server_start> @line<256> msg<Before RcmServer_start> N:VPSS P:2 #:04565 T:00000060cd086b63 S:Module<ti.omx> @<omxrpc_rcm_server_start> @line<258> msg<After RcmServer_start> N:VPSS P:2 #:04566 T:00000060cd08d0e7 S:Instance Register with omxRpc Module.Cnt = 5 N:VPSS P:2 #:04567 T:00000060cd090e17 S:L_create: OmxRpc create: Component:OMX.TI.VPSSM3.CTRL.DC, Layer:2 N:VPSS P:2 #:04568 T:00000060cd09700b S:Component OMX.TI.VPSSM3.CTRL.DC In table OMX.TI.VPSSM3.VFCC idx 0 N:VPSS P:2 #:04569 T:00000060cd09c4d9 S:Component OMX.TI.VPSSM3.CTRL.DC In table OMX.TI.VPSSM3.VFDC idx 1 N:VPSS P:2 #:04570 T:00000060cd0a148d S:Component OMX.TI.VPSSM3.CTRL.DC In table OMX.TI.VPSSM3.VFPC.DEIHDUALOUT idx 2 N:VPSS P:2 #:04571 T:00000060cd0a6ee2 S:Component OMX.TI.VPSSM3.CTRL.DC In table OMX.TI.VPSSM3.VFPC.DEIMDUALOUT idx 3 N:VPSS P:2 #:04572 T:00000060cd0ac6c3 S:Component OMX.TI.VPSSM3.CTRL.DC In table OMX.TI.VPSSM3.VFPC.NF idx 4 N:VPSS P:2 #:04573 T:00000060cd0b2151 S:Component OMX.TI.VPSSM3.CTRL.DC In table OMX.TI.VPSSM3.VFPC.INDTXSCWB idx 5 N:VPSS P:2 #:04574 T:00000060cd0b7aad S:Component OMX.TI.VPSSM3.CTRL.DC In table OMX.TI.VPSSM3.CTRL.TVP idx 6 N:VPSS P:2 #:04575 T:00000060cd0bccf3 S:Component OMX.TI.VPSSM3.CTRL.DC In table OMX.TI.VPSSM3.CTRL.DC idx 7 N:VPSS P:2 #:04576 T:00000060cd0c21ed S:Component OMX.TI.VPSSM3.CTRL.DC found idx: 7 N:VPSS P:2 #:04577 T:00000060cd0c8595 S:In OMX_GetHandle, component OMX.TI.VPSSM3.CTRL.DC, omxhandle 0x9f2a2f40 N:VPSS P:2 #:04578 T:00000060cd0d9131 S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<OMX_BASE_SetDefaultProperties> @line<1238> N:VPSS P:2 #:04579 T:00000060cd0df72b S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<OMX_BASE_SetDefaultProperties> @line<1280> with error<0:ErrorNone> N:VPSS P:2 #:04580 T:00000060cd0e91cf S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<OMX_BASE_ComponentInit> @line<133> N:VPSS P:2 #:04581 T:00000060cd111b25 S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<_OMX_BASE_InitializePorts> @line<115> N:VPSS P:2 #:04582 T:00000060cd11cc23 S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<_OMX_BASE_InitializePorts> @line<217> with error<0:ErrorNone> N:VPSS P:2 #:04583 T:00000060cd17a8d5 S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<OMX_BASE_ComponentInit> @line<247> with error<0:ErrorNone> N:VPSS P:2 #:04584 T:00000060cd1d3db7 S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<OMX_BASE_SetCallbacks> @line<267> N:VPSS P:2 #:04585 T:00000060cd1da215 S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<OMX_BASE_SetCallbacks> @line<308> with error<0:ErrorNone> N:VPSS P:2 #:04586 T:00000060cd1e068d S:Result of pComponentInit: ErrorNone N:VPSS P:2 #:04587 T:00000060cd1e418d S:Registering the component OMX.TI.VPSSM3.CTRL.DC with TunnelMgr N:VPSS P:2 #:04588 T:00000060cd1eacbb S:Entered: DomxTunnelMgr_registerHandle (0x9f2a2f40, 0x9f728654) N:VPSS P:2 #:04589 T:00000060cd1f60af S:Entered function:OmxRpc_rcmClientCreate (0x9f29e2d0, OmxRpcRcmServer_OMX.TI.VPSSM3.CTRL.DC_Cb_3_18, 5) N:VPSS P:2 #:04590 T:00000060cd1fd121 S:Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<983> msg<Before RcmClient_Params_init> N:VPSS P:2 #:04591 T:00000060cd2034c2 S:Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<985> msg<After RcmClient_Params_init> N:VPSS P:2 #:04592 T:00000060cd209203 S:Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<990> msg<Before RcmClient_create> N:VPSS P:2 #:04593 T:00000060cd2adde3 S:Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<992> msg<After RcmClient_create> N:VPSS P:2 #:04594 T:00000060cd2b6b73 S:main: calling RcmClient_getSymbolIndex(OmxRpcCbEventHandler) N:VPSS P:2 #:04595 T:00000060cd4d091b S:main: calling RcmClient_getSymbolIndex(OmxRpcCbEmptyBufferDone) N:VPSS P:2 #:04596 T:00000060cd4ff6d3 S:main: calling RcmClient_getSymbolIndex(OmxRpcCbFillBufferDone) N:VPSS P:2 #:04597 T:00000060cd52c8db S:Module<ti.omx> @<domxtmgr_register_skelinfo> @line<417> msg<OmxRpcRcmServer_OMX.TI.VPSSM3.CTRL.DC_Ctrl_2_16> N:VPSS P:2 #:04598 T:00000060cd536bbd S:OmxRpc_rcmIfGetHandle:ComponentName:OmxRpcRcmServer_OMX.TI.VPSSM3.CTRL.DC_Ctrl_2_16.Exiting.. N:VPSS P:2 #:04599 T:00000060cd9c9a59 S:FATAL ERROR: ErrorCode:0x1. Unhandled Exception: N:VPSS P:2 #:04600 T:00000060cd9ce9ab S:Exception occurred in ThreadType_Task N:VPSS P:2 #:04601 T:00000060cd9d232b S:handle: 0x9f277308. N:VPSS P:2 #:04602 T:00000060cd9d5509 S:stack base: 0x9f277350. N:VPSS P:2 #:04603 T:00000060cd9d897f S:stack size: 0x2000. N:VPSS P:2 #:04604 T:00000060cd9dbbcd S:R0 = 0x9f2a9690 R8 = 0x9f167800 N:VPSS P:2 #:04605 T:00000060cd9dfa9f S:R1 = 0x00000001 R9 = 0x9f279640 N:VPSS P:2 #:04606 T:00000060cd9e37f1 S:R2 = 0x9f5b5021 R10 = 0x9f2a9824 N:VPSS P:2 #:04607 T:00000060cd9e76ab S:R3 = 0x9f583808 R11 = 0x9f27ea80 N:VPSS P:2 #:04608 T:00000060cd9eb50f S:R4 = 0x00028a84 R12 = 0x9f2a9bb8 N:VPSS P:2 #:04609 T:00000060cd9ef2cb S:R5 = 0x00000000 SP(R13) = 0x9f279110 N:VPSS P:2 #:04610 T:00000060cd9f3231 S:R6 = 0x9f167804 LR(R14) = 0x9f5c388d N:VPSS P:2 #:04611 T:00000060cd9f723d S:R7 = 0x9f281a28 PC(R15) = 0x9f5b5090 N:VPSS P:2 #:04612 T:00000060cd9fb1d7 S:PSR = 0x41000000 N:VPSS P:2 #:04613 T:00000060cd9fe397 S:ICSR = 0x00400803 N:VPSS P:2 #:04614 T:00000060cda0164d S:MMFSR = 0x00 N:VPSS P:2 #:04615 T:00000060cda043ef S:BFSR = 0x82 N:VPSS P:2 #:04616 T:00000060cda070bd S:UFSR = 0x0000 N:VPSS P:2 #:04617 T:00000060cda09f05 S:HFSR = 0x40000000 N:VPSS P:2 #:04618 T:00000060cda0d0e5 S:DFSR = 0x00000000 N:VPSS P:2 #:04619 T:00000060cda1012f S:MMAR = 0x00028a84 N:VPSS P:2 #:04620 T:00000060cda13213 S:BFAR = 0x00028a84 N:VPSS P:2 #:04621 T:00000060cda16297 S:AFSR = 0x00000000 N:VPSS P:2 #:04622 T:00000060cda192e7 S:FATAL ERROR: ErrorCode:0x1. Terminating Execution...
N:VPSS P:2 #:02475 T:0000000e12ab4cdf S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_SendCommand> @line<499> N:VPSS P:2 #:02476 T:0000000e12ac0b55 S:OMX_BASE_SendCommand:OMX_CommandStateSet, nParam1: 2 N:VPSS P:2 #:02477 T:0000000e12ac98f5 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_SendCommand> @line<669> with error<0:ErrorNone> N:VPSS P:2 #:02478 T:0000000e12ada5f3 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_CmdEventHandler> @line<434> N:VPSS P:2 #:02479 T:0000000e12ae2bcb S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_PROCESS_CmdEvent> @line<526> N:VPSS P:2 #:02480 T:0000000e12afcf91 S:Module<OMX.TI.VPSSM3.VFDC> @<OMX_BASE_PROCESS_CmdEvent> @line<538> msg<Processing OMX_CommandStateSet> N:VPSS P:2 #:02481 T:0000000e12b041e3 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_HandleStateTransition> @line<316> N:VPSS P:2 #:02482 T:0000000e12b09dcb S:Module<OMX.TI.VPSSM3.VFDC> @<_OMX_BASE_HandleStateTransition> @line<402> msg<Executing to Idle Transition> N:VPSS P:2 #:02483 T:0000000e149b03a9 S:Display Driver Stopped!! N:VPSS P:2 #:02484 T:0000000e14a72d6f S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_CB_ReturnEventNotify> @line<100> N:VPSS P:2 #:02485 T:0000000e14a7ac61 S:Module<OMX.TI.VPSSM3.VFDC> @<OMX_BASE_CB_ReturnEventNotify> @line<115> msg<Notify client for state transition> N:VPSS P:2 #:02486 T:0000000e14a832a1 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_CB_ReturnEventNotify> @line<224> with error<0:ErrorNone> N:VPSS P:2 #:02487 T:0000000e14a89fcb S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_HandleStateTransition> @line<483> with error<0:ErrorNone> N:VPSS P:2 #:02488 T:0000000e14a90f7b S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_PROCESS_CmdEvent> @line<784> with error<0:ErrorNone> N:VPSS P:2 #:02489 T:0000000e14a97b53 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_CmdEventHandler> @line<466> with error<0:ErrorNone> N:VPSS P:2 #:02490 T:0000000e14a9f92b S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_CmdCompleteEventHandler> @line<483> N:VPSS P:2 #:02491 T:0000000e14aa527d S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_PROCESS_CmdCompleteEvent> @line<809> N:VPSS P:2 #:02492 T:0000000e14aab10c S:Module<OMX.TI.VPSSM3.VFDC> @<OMX_BASE_PROCESS_CmdCompleteEvent> @line<821> msg<Processing OMX_CommandStateSet> N:VPSS P:2 #:02493 T:0000000e14ab237b S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_HandleStateTransitionComplete> @line<506> N:VPSS P:2 #:02494 T:0000000e14ab888d S:Module<OMX.TI.VPSSM3.VFDC> @<_OMX_BASE_HandleStateTransitionComplete> @line<631> msg<Executing to Idle Transition> N:VPSS P:2 #:02495 T:0000000e14ac0109 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Control> @line<455> N:VPSS P:2 #:02496 T:0000000e14ac6893 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Control> @line<463> with error<0:ErrorNone> N:VPSS P:2 #:02497 T:0000000e14acc903 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Control> @line<455> N:VPSS P:2 #:02498 T:0000000e14ad2203 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Control> @line<463> with error<0:ErrorNone> N:VPSS P:2 #:02499 T:0000000e14ad8e4b S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_HandleStateTransitionComplete> @line<704> with error<0:ErrorNone> N:VPSS P:2 #:02500 T:0000000e14ae2f45 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_EventNotifyToClient> @line<881> N:VPSS P:2 #:02501 T:0000000e14b111db S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_EventNotifyToClient> @line<1172> with error<0:ErrorNone> N:VPSS P:2 #:02502 T:0000000e14b19021 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_PROCESS_CmdCompleteEvent> @line<930> with error<0:ErrorNone> N:VPSS P:2 #:02503 T:0000000e14b1fb45 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_CmdCompleteEventHandler> @line<496> with error<0:ErrorNone> N:VPSS P:2 #:02504 T:0000000e14b2669d S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_CmdEventHandler> @line<434> N:VPSS P:2 #:02505 T:0000000e14b2d257 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_CmdEventHandler> @line<466> with error<0:ErrorNone> N:VPSS P:2 #:02506 T:0000000e14e4ef01 S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<OMX_BASE_SendCommand> @line<499> N:VPSS P:2 #:02507 T:0000000e14e5c305 S:OMX_BASE_SendCommand:OMX_CommandStateSet, nParam1: 2 N:VPSS P:2 #:02508 T:0000000e14e66379 S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<OMX_BASE_SendCommand> @line<669> with error<0:ErrorNone> N:VPSS P:2 #:02509 T:0000000e14e78a3d S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<OMX_BASE_CmdEventHandler> @line<434> N:VPSS P:2 #:02510 T:0000000e14e81725 S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<OMX_BASE_PROCESS_CmdEvent> @line<526> N:VPSS P:2 #:02511 T:0000000e14e9edcf S:Module<OMX.TI.VPSSM3.CTRL.DC> @<OMX_BASE_PROCESS_CmdEvent> @line<538> msg<Processing OMX_CommandStateSet> N:VPSS P:2 #:02512 T:0000000e14ea6877 S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<_OMX_BASE_HandleStateTransition> @line<316> N:VPSS P:2 #:02513 T:0000000e14eb0933 S:Module<OMX.TI.VPSSM3.CTRL.DC> @<_OMX_BASE_HandleStateTransition> @line<402> msg<Executing to Idle Transition> N:VPSS P:2 #:02514 T:0000000e14eb9605 S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<OMX_BASE_CB_ReturnEventNotify> @line<100> N:VPSS P:2 #:02515 T:0000000e14ebf9a1 S:Module<OMX.TI.VPSSM3.CTRL.DC> @<OMX_BASE_CB_ReturnEventNotify> @line<115> msg<Notify client for state transition> N:VPSS P:2 #:02516 T:0000000e14ec79d7 S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<OMX_BASE_CB_ReturnEventNotify> @line<224> with error<0:ErrorNone> N:VPSS P:2 #:02517 T:0000000e14ece7f5 S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<_OMX_BASE_HandleStateTransition> @line<483> with error<0:ErrorNone> N:VPSS P:2 #:02518 T:0000000e14ed5309 S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<OMX_BASE_PROCESS_CmdEvent> @line<784> with error<0:ErrorNone> N:VPSS P:2 #:02519 T:0000000e14edc067 S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<OMX_BASE_CmdEventHandler> @line<466> with error<0:ErrorNone> N:VPSS P:2 #:02520 T:0000000e14ee3871 S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<OMX_BASE_CmdCompleteEventHandler> @line<483> N:VPSS P:2 #:02521 T:0000000e14ee9669 S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<OMX_BASE_PROCESS_CmdCompleteEvent> @line<809> N:VPSS P:2 #:02522 T:0000000e14eef22f S:Module<OMX.TI.VPSSM3.CTRL.DC> @<OMX_BASE_PROCESS_CmdCompleteEvent> @line<821> msg<Processing OMX_CommandStateSet> N:VPSS P:2 #:02523 T:0000000e14ef64a7 S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<_OMX_BASE_HandleStateTransitionComplete> @line<506> N:VPSS P:2 #:02524 T:0000000e14efc88d S:Module<OMX.TI.VPSSM3.CTRL.DC> @<_OMX_BASE_HandleStateTransitionComplete> @line<631> msg<Executing to Idle Transition> N:VPSS P:2 #:02525 T:0000000e14f03e73 S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<_OMX_BASE_HandleStateTransitionComplete> @line<704> with error<0:ErrorNone> N:VPSS P:2 #:02526 T:0000000e14f0b289 S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<_OMX_BASE_EventNotifyToClient> @line<881> N:VPSS P:2 #:02527 T:0000000e14f3adb7 S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<_OMX_BASE_EventNotifyToClient> @line<1172> with error<0:ErrorNone> N:VPSS P:2 #:02528 T:0000000e14f42921 S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<OMX_BASE_PROCESS_CmdCompleteEvent> @line<930> with error<0:ErrorNone> N:VPSS P:2 #:02529 T:0000000e14f4970b S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<OMX_BASE_CmdCompleteEventHandler> @line<496> with error<0:ErrorNone> N:VPSS P:2 #:02530 T:0000000e14f507d1 S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<OMX_BASE_CmdEventHandler> @line<434> N:VPSS P:2 #:02531 T:0000000e14f56f0b S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<OMX_BASE_CmdEventHandler> @line<466> with error<0:ErrorNone> N:VPSS P:2 #:02532 T:0000000e15397889 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_SendCommand> @line<499> N:VPSS P:2 #:02533 T:0000000e153a3460 S:OMX_BASE_SendCommand:OMX_CommandStateSet, nParam1: 1 N:VPSS P:2 #:02534 T:0000000e153ac37d S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_SendCommand> @line<669> with error<0:ErrorNone> N:VPSS P:2 #:02535 T:0000000e153bbe5b S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_CmdEventHandler> @line<434> N:VPSS P:2 #:02536 T:0000000e153c3ed7 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_PROCESS_CmdEvent> @line<526> N:VPSS P:2 #:02537 T:0000000e153d6ca3 S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02538 T:0000000e153ff7dd S:Module<OMX.TI.VPSSM3.VFDC> @<OMX_BASE_PROCESS_CmdEvent> @line<538> msg<Processing OMX_CommandStateSet> N:VPSS P:2 #:02539 T:0000000e15408343 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_HandleStateTransition> @line<316> N:VPSS P:2 #:02541 T:0000000e1541ff2d S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02540 T:0000000e1540df17 S:Module<OMX.TI.VPSSM3.VFDC> @<_OMX_BASE_HandleStateTransition> @line<367> msg<Idle to Loaded Transition> N:VPSS P:2 #:02542 T:0000000e1545cc37 S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02543 T:0000000e15499fdb S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02544 T:0000000e154c027d S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_CB_ReturnEventNotify> @line<100> N:VPSS P:2 #:02545 T:0000000e154c78e7 S:Module<OMX.TI.VPSSM3.VFDC> @<OMX_BASE_CB_ReturnEventNotify> @line<115> msg<Notify client for state transition> N:VPSS P:2 #:02546 T:0000000e154d0289 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_CB_ReturnEventNotify> @line<224> with error<0:ErrorNone> N:VPSS P:2 #:02547 T:0000000e154d7037 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_HandleStateTransition> @line<483> with error<0:ErrorNone> N:VPSS P:2 #:02548 T:0000000e154e12b3 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_PROCESS_CmdEvent> @line<784> with error<0:ErrorNone> N:VPSS P:2 #:02550 T:0000000e154f73ed S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02549 T:0000000e154e8513 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_CmdEventHandler> @line<466> with error<0:ErrorNone> N:VPSS P:2 #:02551 T:0000000e1551e511 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_CmdCompleteEventHandler> @line<483> N:VPSS P:2 #:02553 T:0000000e15531c74 S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02552 T:0000000e15523fd3 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_PROCESS_CmdCompleteEvent> @line<809> N:VPSS P:2 #:02554 T:0000000e1555666f S:Module<OMX.TI.VPSSM3.VFDC> @<OMX_BASE_PROCESS_CmdCompleteEvent> @line<821> msg<Processing OMX_CommandStateSet> N:VPSS P:2 #:02555 T:0000000e1556b706 S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02556 T:0000000e1558b251 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_HandleStateTransitionComplete> @line<506> N:VPSS P:2 #:02557 T:0000000e155926df S:Module<OMX.TI.VPSSM3.VFDC> @<_OMX_BASE_HandleStateTransitionComplete> @line<595> msg<Idle to Loaded Transition> N:VPSS P:2 #:02558 T:0000000e155a5a1b S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02559 T:0000000e155c6675 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_HandleStateTransitionComplete> @line<704> with error<0:ErrorNone> N:VPSS P:2 #:02561 T:0000000e155e1a25 S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02560 T:0000000e155ce3e3 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_EventNotifyToClient> @line<881> N:VPSS P:2 #:02562 T:0000000e1561e64b S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02563 T:0000000e1565bea1 S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02564 T:0000000e1569669f S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02565 T:0000000e156d5de7 S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02566 T:0000000e15709e2f S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02567 T:0000000e1573cf23 S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02568 T:0000000e1577e52d S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02569 T:0000000e157d67eb S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02570 T:0000000e15847dc4 S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02571 T:0000000e158f1c79 S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02572 T:0000000e15961a01 S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02573 T:0000000e15a06b23 S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02574 T:0000000e15a8be37 S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02575 T:0000000e15aff0f5 S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02576 T:0000000e15b33e45 S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02577 T:0000000e15b64b83 S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02578 T:0000000e15b9818d S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02579 T:0000000e15bcad5d S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02580 T:0000000e15bfcb81 S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02581 T:0000000e16100051 S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02582 T:0000000e16142f3f S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02583 T:0000000e161867c9 S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02584 T:0000000e1627e873 S:Entered Function :omxrpc_skel_freebuffer N:VPSS P:2 #:02585 T:0000000e162a1c3b S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Close> @line<275> N:VPSS P:2 #:02586 T:0000000e162eff15 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Close> @line<283> with error<0:ErrorNone> N:VPSS P:2 #:02587 T:0000000e162f7569 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Deinit> @line<189> N:VPSS P:2 #:02588 T:0000000e162fe857 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Deinit> @line<200> with error<0:ErrorNone> N:VPSS P:2 #:02589 T:0000000e16305b7b S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Close> @line<275> N:VPSS P:2 #:02590 T:0000000e16347beb S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Close> @line<283> with error<0:ErrorNone> N:VPSS P:2 #:02591 T:0000000e1634f3b7 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Deinit> @line<189> N:VPSS P:2 #:02592 T:0000000e1635647d S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Deinit> @line<200> with error<0:ErrorNone> N:VPSS P:2 #:02593 T:0000000e163872d3 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_EventNotifyToClient> @line<1172> with error<0:ErrorNone> N:VPSS P:2 #:02594 T:0000000e1638f1a9 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_PROCESS_CmdCompleteEvent> @line<930> with error<0:ErrorNone> N:VPSS P:2 #:02595 T:0000000e16396149 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_CmdCompleteEventHandler> @line<496> with error<0:ErrorNone> N:VPSS P:2 #:02596 T:0000000e1639d269 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_CmdEventHandler> @line<434> N:VPSS P:2 #:02597 T:0000000e163a3903 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_CmdEventHandler> @line<466> with error<0:ErrorNone> N:VPSS P:2 #:02598 T:0000000e167e0079 S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<OMX_BASE_SendCommand> @line<499> N:VPSS P:2 #:02599 T:0000000e167ec123 S:OMX_BASE_SendCommand:OMX_CommandStateSet, nParam1: 1 N:VPSS P:2 #:02600 T:0000000e167f717b S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<OMX_BASE_SendCommand> @line<669> with error<0:ErrorNone> N:VPSS P:2 #:02601 T:0000000e16807a15 S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<OMX_BASE_CmdEventHandler> @line<434> N:VPSS P:2 #:02602 T:0000000e1680fdb5 S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<OMX_BASE_PROCESS_CmdEvent> @line<526> N:VPSS P:2 #:02603 T:0000000e1682787b S:Module<OMX.TI.VPSSM3.CTRL.DC> @<OMX_BASE_PROCESS_CmdEvent> @line<538> msg<Processing OMX_CommandStateSet> N:VPSS P:2 #:02604 T:0000000e1682ecfd S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<_OMX_BASE_HandleStateTransition> @line<316> N:VPSS P:2 #:02605 T:0000000e1683498f S:Module<OMX.TI.VPSSM3.CTRL.DC> @<_OMX_BASE_HandleStateTransition> @line<367> msg<Idle to Loaded Transition> N:VPSS P:2 #:02606 T:0000000e1684b783 S:Display Controller Path configured for 0!! N:VPSS P:2 #:02607 T:0000000e16850fef S:Display Controller Driver Deleted N:VPSS P:2 #:02608 T:0000000e16854951 S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<OMX_BASE_CB_ReturnEventNotify> @line<100> N:VPSS P:2 #:02609 T:0000000e1685ac3f S:Module<OMX.TI.VPSSM3.CTRL.DC> @<OMX_BASE_CB_ReturnEventNotify> @line<115> msg<Notify client for state transition> N:VPSS P:2 #:02610 T:0000000e16862a8f S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<OMX_BASE_CB_ReturnEventNotify> @line<224> with error<0:ErrorNone> N:VPSS P:2 #:02611 T:0000000e16869955 S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<_OMX_BASE_HandleStateTransition> @line<483> with error<0:ErrorNone> N:VPSS P:2 #:02612 T:0000000e1687333d S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<OMX_BASE_PROCESS_CmdEvent> @line<784> with error<0:ErrorNone> N:VPSS P:2 #:02613 T:0000000e1687a0b7 S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<OMX_BASE_CmdEventHandler> @line<466> with error<0:ErrorNone> N:VPSS P:2 #:02614 T:0000000e16881747 S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<OMX_BASE_CmdCompleteEventHandler> @line<483> N:VPSS P:2 #:02615 T:0000000e16887547 S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<OMX_BASE_PROCESS_CmdCompleteEvent> @line<809> N:VPSS P:2 #:02616 T:0000000e1688d11f S:Module<OMX.TI.VPSSM3.CTRL.DC> @<OMX_BASE_PROCESS_CmdCompleteEvent> @line<821> msg<Processing OMX_CommandStateSet> N:VPSS P:2 #:02617 T:0000000e168943f7 S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<_OMX_BASE_HandleStateTransitionComplete> @line<506> N:VPSS P:2 #:02618 T:0000000e1689a81b S:Module<OMX.TI.VPSSM3.CTRL.DC> @<_OMX_BASE_HandleStateTransitionComplete> @line<595> msg<Idle to Loaded Transition> N:VPSS P:2 #:02619 T:0000000e168a1d21 S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<_OMX_BASE_HandleStateTransitionComplete> @line<704> with error<0:ErrorNone> N:VPSS P:2 #:02620 T:0000000e168a9131 S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<_OMX_BASE_EventNotifyToClient> @line<881> N:VPSS P:2 #:02621 T:0000000e168dc9e5 S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<_OMX_BASE_EventNotifyToClient> @line<1172> with error<0:ErrorNone> N:VPSS P:2 #:02622 T:0000000e168e468d S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<OMX_BASE_PROCESS_CmdCompleteEvent> @line<930> with error<0:ErrorNone> N:VPSS P:2 #:02623 T:0000000e168ed725 S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<OMX_BASE_CmdCompleteEventHandler> @line<496> with error<0:ErrorNone> N:VPSS P:2 #:02624 T:0000000e168f4291 S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<OMX_BASE_CmdEventHandler> @line<434> N:VPSS P:2 #:02625 T:0000000e168fa7b5 S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<OMX_BASE_CmdEventHandler> @line<466> with error<0:ErrorNone> N:VPSS P:2 #:02626 T:0000000e16dbdacf S:OmxRpc_rcmIfFreeHandle:Entered.. N:VPSS P:2 #:02627 T:0000000e1718d317 S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<OMX_BASE_ComponentDeinit> @line<400> N:VPSS P:2 #:02628 T:0000000e17193d2f S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<_OMX_BASE_DeinitializePorts> @line<237> N:VPSS P:2 #:02629 T:0000000e1719c7a3 S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<_OMX_BASE_DeinitializePorts> @line<299> with error<0:ErrorNone> N:VPSS P:2 #:02630 T:0000000e1758b26f S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<OMX_BASE_ComponentDeinit> @line<474> with error<0:ErrorNone> N:VPSS P:2 #:02631 T:0000000e175b8c9d S:Instance UnRegister with omxRpc Module.Cnt = 4 N:VPSS P:2 #:02632 T:0000000e175f5e81 S:OmxRpc_rcmIfFreeHandle:Exiting.. N:VPSS P:2 #:02633 T:0000000e177ff60d S:OmxRpc_rcmIfFreeHandle:Entered.. N:VPSS P:2 #:02634 T:0000000e17807ed5 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_ComponentDeinit> @line<400> N:VPSS P:2 #:02635 T:0000000e1780dd4f S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DeinitializePorts> @line<237> N:VPSS P:2 #:02636 T:0000000e1788acf5 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DeinitializePorts> @line<299> with error<0:ErrorNone> N:VPSS P:2 #:02637 T:0000000e17c14551 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_ComponentDeinit> @line<474> with error<0:ErrorNone> N:VPSS P:2 #:02638 T:0000000e17c685cf S:Instance UnRegister with omxRpc Module.Cnt = 3 N:VPSS P:2 #:02639 T:0000000e17c9c261 S:OmxRpc_rcmIfFreeHandle:Exiting.. N:VPSS P:2 #:02640 T:0000000e185a8ed7 S:OmxRpc_rcmIfGetHandle:ComponentName:OMX.TI.VPSSM3.VFDC N:VPSS P:2 #:02641 T:0000000e185b4f5d S:Entered function:omxrpc_module_init_client (3) N:VPSS P:2 #:02642 T:0000000e185ba3d1 S:LayerId: 2 N:VPSS P:2 #:02643 T:0000000e185c333d S:@ omxrpc_rcm_server_create: rcmServerName OmxRpcRcmServer_OMX.TI.VPSSM3.VFDC_Ctrl_2_9, priority 14 N:VPSS P:2 #:02644 T:0000000e185c9fdf S:Module<ti.omx> @<omxrpc_rcm_server_create> @line<225> msg<Before RcmServer_Params_init> N:VPSS P:2 #:02645 T:0000000e185d05a9 S:Module<ti.omx> @<omxrpc_rcm_server_create> @line<229> msg<After RcmServer_Params_init> N:VPSS P:2 #:02646 T:0000000e185d6177 S:Module<ti.omx> @<omxrpc_rcm_server_create> @line<232> msg<Before RcmServer_create> N:VPSS P:2 #:02647 T:0000000e18639395 S:Module<ti.omx> @<omxrpc_rcm_server_create> @line<240> msg<After RcmServer_create> N:VPSS P:2 #:02648 T:0000000e186400bd S:@ omxrpc_rcm_server_remote_fxn_register regFxnCategory 1 N:VPSS P:2 #:02649 T:0000000e186454a5 S:Calling RcmServer_addSymbol(OmxRpcSetParameter) N:VPSS P:2 #:02650 T:0000000e1864d9cd S:Calling RcmServer_addSymbol(OmxRpcGetParameter) N:VPSS P:2 #:02651 T:0000000e186531c6 S:Calling RcmServer_addSymbol(OmxRpcSetConfig) N:VPSS P:2 #:02652 T:0000000e186592b7 S:Calling RcmServer_addSymbol(OmxRpcGetConfig) N:VPSS P:2 #:02653 T:0000000e1865ebaf S:Calling RcmServer_addSymbol(OmxRpcGetComponentVersion) N:VPSS P:2 #:02654 T:0000000e18666445 S:Calling RcmServer_addSymbol(OmxRpcGetExtensionIndex) N:VPSS P:2 #:02655 T:0000000e1866e0eb S:Calling RcmServer_addSymbol(OmxRpcGetState) N:VPSS P:2 #:02656 T:0000000e186797cf S:Calling RcmServer_addSymbol(OmxRpcSendCommand) N:VPSS P:2 #:02657 T:0000000e186812a1 S:Calling RcmServer_addSymbol(OmxRpcUseBuffer) N:VPSS P:2 #:02658 T:0000000e186874f3 S:Calling RcmServer_addSymbol(OmxRpcAllocBuffer) N:VPSS P:2 #:02659 T:0000000e1868cbad S:Calling RcmServer_addSymbol(OmxRpcFreeBuffer) N:VPSS P:2 #:02660 T:0000000e1869225f S:Calling RcmServer_addSymbol(OmxRpcEmptyThisBuffer) N:VPSS P:2 #:02661 T:0000000e18698053 S:Calling RcmServer_addSymbol(OmxRpcFillThisBuffer) N:VPSS P:2 #:02662 T:0000000e1869f5eb S:Calling RcmServer_addSymbol(OmxRpcTunnelRequest) N:VPSS P:2 #:02663 T:0000000e186a7cdf S:Module<ti.omx> @<omxrpc_rcm_server_start> @line<256> msg<Before RcmServer_start> N:VPSS P:2 #:02664 T:0000000e186b4cb5 S:Module<ti.omx> @<omxrpc_rcm_server_start> @line<258> msg<After RcmServer_start> N:VPSS P:2 #:02665 T:0000000e186bb2d7 S:Instance Register with omxRpc Module.Cnt = 4 N:VPSS P:2 #:02666 T:0000000e186bf2cb S:L_create: OmxRpc create: Component:OMX.TI.VPSSM3.VFDC, Layer:2 N:VPSS P:2 #:02667 T:0000000e186c536b S:Component OMX.TI.VPSSM3.VFDC In table OMX.TI.VPSSM3.VFCC idx 0 N:VPSS P:2 #:02668 T:0000000e186ca6d3 S:Component OMX.TI.VPSSM3.VFDC In table OMX.TI.VPSSM3.VFDC idx 1 N:VPSS P:2 #:02669 T:0000000e186cf943 S:Component OMX.TI.VPSSM3.VFDC found idx: 1 N:VPSS P:2 #:02670 T:0000000e186d62c1 S:In OMX_GetHandle, component OMX.TI.VPSSM3.VFDC, omxhandle 0x9f225750 N:VPSS P:2 #:02671 T:0000000e1872c18b S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_SetDefaultProperties> @line<1238> N:VPSS P:2 #:02672 T:0000000e18734e11 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_SetDefaultProperties> @line<1280> with error<0:ErrorNone> N:VPSS P:2 #:02673 T:0000000e1873b613 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_ComponentInit> @line<133> N:VPSS P:2 #:02674 T:0000000e1875a765 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_InitializePorts> @line<115> N:VPSS P:2 #:02675 T:0000000e1883a1a1 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_InitializePorts> @line<217> with error<0:ErrorNone> N:VPSS P:2 #:02676 T:0000000e18999e2f S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_ComponentInit> @line<247> with error<0:ErrorNone> N:VPSS P:2 #:02677 T:0000000e189a71f1 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:02678 T:0000000e189acdb5 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:02679 T:0000000e189b3fbf S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:02680 T:0000000e189baf01 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:02681 T:0000000e189c2551 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:02682 T:0000000e189c7829 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:02683 T:0000000e189d0319 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:02684 T:0000000e189d7537 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:02685 T:0000000e189dea13 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:02686 T:0000000e189e3dc5 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:02687 T:0000000e189ea52f S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:02688 T:0000000e189f137d S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:02689 T:0000000e189f82ef S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:02690 T:0000000e189fd597 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:02691 T:0000000e18a03cb7 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:02692 T:0000000e18a0aa63 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:02693 T:0000000e18a11a45 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:02694 T:0000000e18a16ccb S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:02695 T:0000000e18a1d537 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:02696 T:0000000e18a242c1 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:02697 T:0000000e18a2b6df S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:02698 T:0000000e18a30975 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:02699 T:0000000e18a3721b S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:02700 T:0000000e18a3e019 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:02701 T:0000000e18a44f6f S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:02702 T:0000000e18a4bdd3 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:02703 T:0000000e18a526b5 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:02704 T:0000000e18a59449 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:02705 T:0000000e18a607c9 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:02706 T:0000000e18a65a43 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:02707 T:0000000e18a6c1d7 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:02708 T:0000000e18a72f73 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:02709 T:0000000e18a79ea1 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:02710 T:0000000e18a7f133 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:02711 T:0000000e18a858e5 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:02712 T:0000000e18a8c66d S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:02713 T:0000000e18a935a3 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:02714 T:0000000e18a9884b S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:02715 T:0000000e18a9eff7 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:02716 T:0000000e18aa604a S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:02717 T:0000000e18aad163 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:02718 T:0000000e18ab2473 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:02719 T:0000000e18ab8c33 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:02720 T:0000000e18abfaa1 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:02721 T:0000000e18ac8981 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:02722 T:0000000e18acdcf1 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:02723 T:0000000e18ad458f S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:02724 T:0000000e18adb335 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:02725 T:0000000e18ae23fd S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:02726 T:0000000e18ae775b S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:02727 T:0000000e18aede9d S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:02728 T:0000000e18af4c79 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:02729 T:0000000e18afbc6d S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:02730 T:0000000e18b00f4d S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:02731 T:0000000e18b076c1 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:02732 T:0000000e18b0e46d S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:02733 T:0000000e18b155af S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:02734 T:0000000e18b1a9cd S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:02735 T:0000000e18b213a1 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:02736 T:0000000e18b28295 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:02737 T:0000000e18b2f473 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:02738 T:0000000e18b347c7 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:02739 T:0000000e18b3ca1d S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:02740 T:0000000e18b43c25 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:02741 T:0000000e18b4b011 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:02742 T:0000000e18b50395 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:02743 T:0000000e18b56b19 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:02744 T:0000000e18b5d8f9 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:02745 T:0000000e18b64669 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:02746 T:0000000e18b6995f S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:02747 T:0000000e18b7019a S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:02748 T:0000000e18b76fab S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:02749 T:0000000e18b7deb9 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:02750 T:0000000e18b832ab S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:02751 T:0000000e18b899e1 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:02752 T:0000000e18b9076d S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:02753 T:0000000e18b979c1 S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546> N:VPSS P:2 #:02754 T:0000000e18b9cc71 S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<626> N:VPSS P:2 #:02755 T:0000000e18ba3461 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<690> with error<0:ErrorNone> N:VPSS P:2 #:02756 T:0000000e18baa295 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:ErrorNone> N:VPSS P:2 #:02757 T:0000000e18bb0c8b S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_SetCallbacks> @line<267> N:VPSS P:2 #:02758 T:0000000e18bb8c29 S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_SetCallbacks> @line<308> with error<0:ErrorNone> N:VPSS P:2 #:02759 T:0000000e18bbf4bf S:Result of pComponentInit: ErrorNone N:VPSS P:2 #:02760 T:0000000e18bc2f63 S:Registering the component OMX.TI.VPSSM3.VFDC with TunnelMgr N:VPSS P:2 #:02761 T:0000000e18bc7853 S:Entered: DomxTunnelMgr_registerHandle (0x9f225750, 0x9f728ad4) N:VPSS P:2 #:02762 T:0000000e18bd1ceb S:Entered function:OmxRpc_rcmClientCreate (0x9f220b40, OmxRpcRcmServer_OMX.TI.VPSSM3.VFDC_Cb_3_11, 5) N:VPSS P:2 #:02763 T:0000000e18bd88f9 S:Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<983> msg<Before RcmClient_Params_init> N:VPSS P:2 #:02764 T:0000000e18bdebab S:Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<985> msg<After RcmClient_Params_init> N:VPSS P:2 #:02765 T:0000000e18be4857 S:Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<990> msg<Before RcmClient_create> N:VPSS P:2 #:02766 T:0000000e18c6544b S:Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<992> msg<After RcmClient_create> N:VPSS P:2 #:02767 T:0000000e18c6e01f S:main: calling RcmClient_getSymbolIndex(OmxRpcCbEventHandler) N:VPSS P:2 #:02768 T:0000000e18cab9cd S:main: calling RcmClient_getSymbolIndex(OmxRpcCbEmptyBufferDone) N:VPSS P:2 #:02769 T:0000000e18cf754f S:FATAL ERROR: ErrorCode:0x1. Unhandled Exception: N:VPSS P:2 #:02770 T:0000000e18cfbf17 S:Exception occurred in ThreadType_Task N:VPSS P:2 #:02771 T:0000000e18cff6d5 S:handle: 0x9f24bc88. N:VPSS P:2 #:02772 T:0000000e18d02c0f S:stack base: 0x9f24bcd0. N:VPSS P:2 #:02773 T:0000000e18d0620f S:stack size: 0x2000. N:VPSS P:2 #:02774 T:0000000e18d096ab S:R0 = 0x9f29e9f0 R8 = 0x9f167800 N:VPSS P:2 #:02775 T:0000000e18d0d707 S:R1 = 0x00000001 R9 = 0x9f24dfc0 N:VPSS P:2 #:02776 T:0000000e18d11517 S:R2 = 0x9f5b5021 R10 = 0x9f29eb84 N:VPSS P:2 #:02777 T:0000000e18d15473 S:R3 = 0x9f583808 R11 = 0x9f253400 N:VPSS P:2 #:02778 T:0000000e18d193e7 S:R4 = 0x00028f04 R12 = 0x9f29efb8 N:VPSS P:2 #:02779 T:0000000e18d1d2a7 S:R5 = 0x00000000 SP(R13) = 0x9f24da90 N:VPSS P:2 #:02780 T:0000000e18d2137b S:R6 = 0x9f167804 LR(R14) = 0x9f5c388d N:VPSS P:2 #:02781 T:0000000e18d254a7 S:R7 = 0x9f281a38 PC(R15) = 0x9f5b5090 N:VPSS P:2 #:02782 T:0000000e18d29571 S:PSR = 0x41000000 N:VPSS P:2 #:02783 T:0000000e18d2c7e5 S:ICSR = 0x0440f803 N:VPSS P:2 #:02784 T:0000000e18d2f8d1 S:MMFSR = 0x00 N:VPSS P:2 #:02785 T:0000000e18d324e3 S:BFSR = 0x82 N:VPSS P:2 #:02786 T:0000000e18d352bf S:UFSR = 0x0000 N:VPSS P:2 #:02787 T:0000000e18d381c5 S:HFSR = 0x40000000 N:VPSS P:2 #:02788 T:0000000e18d3b48f S:DFSR = 0x00000000 N:VPSS P:2 #:02789 T:0000000e18d3e5cb S:MMAR = 0x00028f04 N:VPSS P:2 #:02790 T:0000000e18d4179b S:BFAR = 0x00028f04 N:VPSS P:2 #:02791 T:0000000e18d448ef S:AFSR = 0x00000000 N:VPSS P:2 #:02792 T:0000000e18d47a1f S:FATAL ERROR: ErrorCode:0x1. Terminating Execution...