Given the Boot loader is actually in ROM but not advised to use with the I2C or SPI port .. could our secondary boot code set-up the I2C or SPI port and then call the boot loader function in ROM ? In other words is the ROM Boot loader function “callable” ? ... Is it possible to call the AIS functions in ROM just like we can call DSP functions in ROM?