This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c6745 initialisation



Hi,
it’s the first time for me working with a DSP and CCS. It would be very kind of you, if you can give me some hints what I can do.
I have a C6745 on a custom board. For the Connection I am using a Spectrum Digital XDS100V2. The JTAG Connection Test of CCS is successful.
I am using this GEL File for my DSP:

When I start the Debugger, I get a Message like “Trouble writing Memory at …”. The Problem occurs at the line 503 in the Setup_System_Config function:
KICK0R = 0x83e70b13; // Kick0 register + data (unlock)

I think the Hardware runs correctly. I have already checked the supply voltages. Regards,

Holger Klaus