This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ATA_write bug ????

Hi everyone,

I wonder if anyone had ever written large file (nearly 2 MB) on SD card using ATA_write function. I tried to write 2 different files and encountered a mystery. After wrtting 2048 words  correctly, the next 256 words (one write buffer size) were wrong (each word was shifted 8-bit to the left), this problem repeated until the end of file.

  • Hi,

    I had the same problem as you, but i noticed that if i start by writing only some bytes (8), after closing and re opening it i can write correctly without any problem. 

    I don't have any explanation but it works.

    try it, if you still having the same problem, we ill try to resolve it together.