Other Parts Discussed in Thread: AM3517
I'm attempting to build the OCF drivers for the AM3517. I'm using the ti-sdk-am3517-evm-05.04.00.00 SDK. I'm looking at the instructions on the Crypto Wiki page here:
When I build the drivers with these commands:
make ti-ocf-crypto-module
make ti-ocf-crypto-module_install
the wiki seems to say that both cryptodev.ko and ocf_omap3_cryptok.ko should be added to the rootfs. There are no errors with my build/install but cryptodev.ko is not installed. Only ocf_omap3_cryptok.ko is added to the rootFS
Also, when you move on to the Build OCF for Sitara section, it's written for the 03.00.01.06 PSP which is not in the current release of the SDK. Has anyone gotten this working for the 05.04.00.00/04.02.00.07 SDK/PSP. If so, which releases of ocf-linux and crypto-tools did you use?
Thanks,
Jemiah
.