Other Parts Discussed in Thread: 4430
Hi all,
We are working on ICS bring-up on PandaboardES which is based on OMAP4460.
I followed the instructions which are mentioned in the below link. (master branch - ICS, AOSP kernel, Xloader and Uboot)
http://www.omapedia.org/wiki/Android_Panda_Build_Source
But, when i tried to boot it from the SDCARD, the system is getting repeatedly booted up.
Even the pre-built images are also throwing the same error.
http://www.omapedia.org/wiki/Android_Panda_Pre_Built
Can someone provide the link to download the
a) Kernel source code
b) U-Boot and X-loader
c) Android File System (ICS)
for PandboardES which is running on OMAP4460
Regards
Sandeep S.P