This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Flashing IBL for PCIe Boot example failed

Hello,

I've tried to flash the IBL for the PCIe Boot example, but it always fails while verifying the data (see below). I just followed these instructions and everything works fine: http://processors.wiki.ti.com/index.php/BIOS_MCSDK_2.0_User_Guide#IBL

I'm using CCS5.1.1.00028 and MCSDK 2.00.08.20. Can somebody help?

Best Regards,
Bernd

PS: next I'll be on holiday so I can't answer at once

[C66xx_0] EEPROM Writer Utility Version 01.00.00.04
[C66xx_0]
[C66xx_0] Writing 51932 bytes from DSP memory address 0x80000000 to EEPROM bus address 0x0051 starting from device address 0x0000 ...
[C66xx_0] Reading 51932 bytes from EEPROM bus address 0x0051 to DSP memory address 0x80010000 starting from device address 0x0000 ...
[C66xx_0] Verifying data read ...
[C66xx_0] Failure at byte 9, expected 0x00000080, read 0x00000080
[C66xx_0] EEPROM read verify failed