This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6670 simulator with NDK: Ping failing



Followed the link http://processors.wiki.ti.com/index.php/BIOS_MCSDK_2.0_User_Guide#Building_and_running_NDK_client_example_with_simulator

to configure the simulator on linux fedora14 with CCSv5 and sys bios 6

The client evm6670 project is built and all the initial test are passed and configured to a staic IP. But still can not ping the DSP from same subnet

[TMS320C66x_0] QMSS successfully initialized
[TMS320C66x_0] CPPI successfully initialized
[TMS320C66x_0] PA successfully initialized
[TMS320C66x_0]
[TMS320C66x_0] TCP/IP Stack Example Client
[TMS320C66x_0] PASS successfully initialized
[TMS320C66x_0] Ethernet subsystem successfully initialized
[TMS320C66x_0] Ethernet eventId : 48 and vectId (Interrupt) : 7
[TMS320C66x_0] Registration of the EMAC Successful, waiting for link up ..
[TMS320C66x_0] Network Added: If-1:10.141.68.251
[TMS320C66x_0] Service Status: Telnet : Enabled : : 000
[TMS320C66x_0] Service Status: HTTP : Enabled : : 000