Hi,
I have a TI816x Netra board with an 816x expansion IO daughter card.
On the daughter card, I have an HDMI port with says "HDMI IN2".
- Is this port meant for HDMI in or DVI capture?
- Which are the Vip ports to which this HDMI/DVI port is connected?
- Is chains example sufficient for capture of data over this interface.
- If it is DVI source, what kind of media sources can I connect to it?
Regards,
Karthik
Is chains example sufficient for capture of data over this interface.