hi, all

I'm trying to debug why running the application built by C6run on Beagle board can make the Linux OS crash. Below is my test process.

First ssh connect to the beagle board, then execute the algorithm once and quit the ssh connection.  Each time the execution of the ARM Linux application built by C6runapp-cc is like this "ssh root@${REMOTEADDR}  \"cd ${REMOTE_DIR}; ${RUN_CMD}; \"", here the RUN_CMD is to run the application. The error message from the kernel is like this

[ 7770.725952] sh invoked oom-killer: gfp_mask=0xd0, order=2, oom_adj=0
[ 7770.732391] [<c003ab54>] (unwind_backtrace+0x0/0xdc) from [<c00b75d0>] (dump_header+0x5c/0x154)
[ 7770.741180] [<c00b75d0>] (dump_header+0x5c/0x154) from [<c00b7704>] (oom_kill_process+0x3c/0xdc)
[ 7770.750305] [<c00b7704>] (oom_kill_process+0x3c/0xdc) from [<c00b7d50>] (__out_of_memory+0x188/0x1ac)
[ 7770.759582] [<c00b7d50>] (__out_of_memory+0x188/0x1ac) from [<c00b7e08>] (out_of_memory+0x94/0xec)
[ 7770.768615] [<c00b7e08>] (out_of_memory+0x94/0xec) from [<c00badb4>] (__alloc_pages_nodemask+0x3e4/0x55c)
[ 7770.778259] [<c00badb4>] (__alloc_pages_nodemask+0x3e4/0x55c) from [<c00baf3c>] (__get_free_pages+0x10/0x3c)
[ 7770.788330] [<c00baf3c>] (__get_free_pages+0x10/0x3c) from [<c003cb98>] (get_pgd_slow+0x14/0xe0)
[ 7770.797180] [<c003cb98>] (get_pgd_slow+0x14/0xe0) from [<c006322c>] (mm_init+0x90/0xcc)
[ 7770.805236] [<c006322c>] (mm_init+0x90/0xcc) from [<c00637f8>] (dup_mm+0x64/0x524)
[ 7770.812866] [<c00637f8>] (dup_mm+0x64/0x524) from [<c006451c>] (copy_process+0x824/0xea8)
[ 7770.821105] [<c006451c>] (copy_process+0x824/0xea8) from [<c0064cfc>] (do_fork+0x15c/0x3ac)
[ 7770.829528] [<c0064cfc>] (do_fork+0x15c/0x3ac) from [<c0035f40>] (ret_fast_syscall+0x0/0x2c)
[ 7770.838043] Mem-info:
[ 7770.840332] Normal per-cpu:
[ 7770.843139] CPU    0: hi:   18, btch:   3 usd:   0
[ 7770.848144] active_anon:208 inactive_anon:412 isolated_anon:0
[ 7770.848144]  active_file:0 inactive_file:23 isolated_file:0
[ 7770.848175]  unevictable:0 dirty:0 writeback:0 unstable:0
[ 7770.848175]  free:1847 slab_reclaimable:386 slab_unreclaimable:947
[ 7770.848175]  mapped:16 shmem:59 pagetables:58 bounce:0
[ 7770.876342] Normal free:7388kB min:1140kB low:1424kB high:1708kB active_anon:832kB inactive_anon:1648kB active_file:0kB inactive_file:92kB unevictable:0kB isolated(anon):0kB isolated(file):0kB present:81280kB mlocked:0kB dirty:0kB writeback:0kB mapped:64kB shmem:236kB slab_reclaimable:1544kB slab_unreclaimable:3788kB kernel_stack:424kB pagetables:232kB unstable:0kB bounce:0kB writeback_tmp:0kB pages_scanned:0 all_unreclaimable? no
[ 7770.914672] lowmem_reserve[]: 0 0
[ 7770.918029] Normal: 761*4kB 507*8kB 16*16kB 1*32kB 0*64kB 0*128kB 0*256kB 0*512kB 0*1024kB 0*2048kB 0*4096kB = 7388kB
[ 7770.928833] 82 total pagecache pages
[ 7770.932434] 0 pages in swap cache
[ 7770.935760] Swap cache stats: add 0, delete 0, find 0/0
[ 7770.941284] Free swap  = 0kB
[ 7770.944183] Total swap = 0kB
[ 7770.949279] 20480 pages of RAM
[ 7770.952423] 2704 free pages
[ 7770.955230] 10318 reserved pages
[ 7770.958465] 1333 slab pages
[ 7770.961273] 63 pages shared
[ 7770.964080] 0 pages swap cached
[ 7770.967254] Out of memory: kill process 10087 (sh) score 988 or a child
[ 7770.973907] Killed process 10089 (enc_c64_beagle_)
Firstly I doubt if the network connection cause this problem, but if I run an ARM-only application, it seems the Linux OS will not crash even I run the application by thousands of times which cost more than one day. But if I replace the ARM-only application with the APP built by C6run, the OS will crash with above error after one or two hours, is there any clue for solution or is it a C6run known bug? 
The application is built by following steps, first, using cgt7.2.2 to build a library contains the core algorithm running on DSP side and then build the executive application using c6run. And the C6run version is 0.94.05.06, which is the default version for dvsdk 4.01.00.09.

Thanks a lot