Hi,
Now I am geting in trouble with the McFw framework. I use link below,but I can not see anything in the SD display screen.
PS: it work fine without the dei link.
Then I add the dei link becase frames can be converted from interlace to the progressive format,
which is better to process using Vlib or OpenCV and so on.
But after I add the dei link to the usecase, It do not work fine.
anyone tell why? The wrong link is below.