Hi,
I have been looking at the AM335x General Purpose EVM schematics for a guide as to how to connect the PWRONRSTn signal of the AM335x.
I noticed the EVM has connected PWRONRSTn to a 1.8V signal based on a Power Management IC output. SPRS717C Table 3.7 specifies that the High Level Voltage threshold for the PWRONRSTn signal is 2V (VDDSHV6 = 3.3V). This is obviously working ok for the EVM but I was wondering if acceptable to drive PWRONRSTn by a 1.8V signal in this case or have I missed something?
Kind Regards
Mark