Other Parts Discussed in Thread: OMAPL138, SYSBIOS
Hi,
I am facing an issue with OMAPL138 DSP SYS/BIOS clock timer settings. I am using TImer2 for DSP Clock (Timer1&2 used by ARM).
The PLL Setting is done for ARM & DSP clock of 300MHz. SYSCLK1 and SYSCLK6 are 300MHz. PLL1_SYSCLK2 used for TIMER2/3 are 150MHz.
(Our OSC clock is 24MHz PLLM = 24 and POSTDIV = 1. gives SYSCLK1/6 = (24x25/2) = 300MHz ).
The kernel boot-up gives the message "Calibrating delay loop... 149.50 BogoMIPS (lpj=747520)", What it means? Is this BogoMIPS is Hlaf of CPU Clock?
When i check the DSP BIOS Frequency, It is giving 300MHz. I checked this by adding the below code snaps in my application:
BIOS_getCpuFreq(&getCpuFreq);
System_printf("Main: BIOS_getCpuFreq = 0x%d\n", getCpuFreq.lo);
Output ==> Main: BIOS_getCpuFreq =0x300000000
Now i am facing some DSP processing Delay issues. If i put Task_Sleep(1000) (ie 1sec sleep) in my DSP task, It is taking 20 -30 seconds (instead of 1 sec)
to come out from the sleep function. I am suspecting some Clock & TImer configuration mismatch between the actual settings and the BIOS configuration.
For further information on my system,
I am using following package versions for my DSP application:
* bios_6_33_02_31
* syslink_2_10_03_20
* ipc_1_24_02_27
* xdctools_3_23_01_43
* CGT_C6000_7.2.2
I have the following clock & Timer configurations in my bios.cfg file.
var Clock = xdc.useModule('ti.sysbios.knl.Clock');
Clock.tickSource = Clock.TickSource_TIMER; // To used timer
Clock.timerId = 2; // this changes the default Timer used by BIOS to 2.
Clock.tickPeriod = 1000; // 1000mS = 1ms (ticks in terms of microseconds )
var Timer = xdc.useModule('ti.sysbios.timers.timer64.Timer');
Timer.intFreqs[2].lo = 149500000; // Setting Timer to ~150Mhz ---> Timer2/3 uses PLL1_SYSCLK2.
Timer.intFreqs[2].hi = 0;
Timer.timerSettings[2].mode = Timer.Mode_CHAINED;
Timer.timerSettings[2].master = true;
Timer.timerSettings[2].ownerCoreId = 0;
I am setting Clock.tickPeriod value as 1000 in my config file. What will be the default value? and for my Timer2 Frequency setting of 150MHz, What value should be configured for Clock.tickPeriod ?
Below is the Timer2 register dump taken after the DSP BIOS started up and Run.
Read at address 0x01F0C000 (0x40316000): 0x4472020C
Read at address 0x01F0C004 (0x401c3004): 0x00000000
Read at address 0x01F0C008 (0x4024b008): 0x00000000
Read at address 0x01F0C00C (0x4008c00c): 0x00000000
Read at address 0x01F0C010 (0x402b9010): 0x0001755E
Read at address 0x01F0C014 (0x4032f014): 0x00000000
Read at address 0x01F0C018 (0x401d8018): 0x000247FC
Read at address 0x01F0C01C (0x4024b01c): 0x00000000
Read at address 0x01F0C020 (0x400ff020): 0x00000090
Read at address 0x01F0C024 (0x400bf024): 0x0000000F
Read at address 0x01F0C028 (0x40277028): 0x00000000
Read at address 0x01F0C02C (0x402cd02c): 0x00000290
Read at address 0x01F0C030 (0x401b3030): 0x00000000
Read at address 0x01F0C034 (0x402c0034): 0x00000000
Read at address 0x01F0C038 (0x4023f038): 0x00000000
Read at address 0x01F0C03C (0x4022f03c): 0x00000000
Read at address 0x01F0C040 (0x4028d040): 0x00000000
Read at address 0x01F0C044 (0x4022d044): 0x00000002
Read at address 0x01F0C048 (0x402db048): 0x00000000
Read at address 0x01F0C04C (0x4016604c): 0x00000000
I have noticed the value of Timer2 Period Register (addr: 0x01F0C018) = 0x000247FC. It Seems to be ok for me for the 149.5MHz input frequency. Please verify this.
Because of the delay issue with DSP, i am facing issue with our current application design and my ARM-DSP integration is getting delayed.
Please guide me to resolve the above issue. Awaiting for your response.
--
Thanks and Regards,
Ansa Ahammed