This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

encoding resolution non-multiply of 16

Hello,

In H.264 encoder datasheet it says :

"Supports image width and height that are multiple of 16, also supports
image height being non-multiple of 16".

What can I do with reolution of 600x600. Is it possible to use this encoder with this frame?

Thank You.