I have a question concerning the CVDD voltage. As I understand it at the moment the CVDD voltage varies from 0.9V to 1.1V from chip to chip, each chip will be programmed with the min. CVDD voltage during manufacturing. This min voltage could be different from chip to chip. The C667x than sends these information during startup via its VID-interface to the voltage controller.
My question now is what happens when I use a 1.25GHz C667x but run it only at 1.0GHz, is than the CVDD voltage which is send from the C667x over the VID interface to the voltage controller lower compared to running at 1.25GHz. Or asked in other words, is the inside the DSP programmed min CVDD a function of the Corefrequency or is it always the same.
Thx,
Markus