This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ICS on DM37x + USB communication



Hey All,

Question 1:  I'm working on getting the TI-Android-ICS-4.0.3-DevKit-3.0.0 working on a DM37x board.  I see that the image supposedly only supports AM37x, yet it supports the Beagleboard XM, which is a DM37x.  Would I have to do anything special to get it running on my board?

Question 2:  I see that the Open Accessory libraries are not yet supported in the release.  Does anyone have an eta of when they will be supported?  Is there any way to do simple USB communication between the Android device and a PC with the current release?

Cheers!

Mark