Other Parts Discussed in Thread: THS8135, THS8200, TPD7S019
THS8135 connction to DM8148.
We are looking for advice on setting up the video output system as a whole, supporting 10-bit video, seperate HSYNC/VSYNC in addition to embedded SYNC's.
1) In our application we want to support 10-bit video. Our first concern is that we were told the DM8148 does support this, but we don't see enough pins on the IC. Can you conform that we do in fact have 10-bit video on the DM8148?
2) We need to provide HSYNC and VSYNC to the DB-15 video connector. These come directly from the DM8148. Should we buffer these or do you suggest driving them out the connector directly from the DM8148? Buffering provides a layer of physical protection, better to blow up a buffer than the DM8148 if a short or something crazy happens!. What do you suggest?
3) We would like to support seperate HSYNC and VSYNC as I mention above, but also the option to embed the SYNC's. This will provide the most system flexability. I see that the THS8135 does support this, can you guide us in connecting this up? It looks like we'll take the HSYNC and VSYNC to the THS8135, but will we need external circuitry to turn them on and off when embedding, or not embedding them? Maybe supporting both modes is popular. Let us know how to hook all of this up.
Thank you,
Bryan Busacco