This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Custon screen resolution on beagleboard not working



Hi guys and girls, got a problem with ICS on the beagleboard-xm. basically iv'e bought the following board and screen online (http://www.chalk-elec.com/?page_id=1280#ecwid:category=0&mode=product&product=7703686) however when i try to set the resolution to the specified 1024x600  it seems to defualt to 1024x768 but then if i set to 800x600 it sets to the proper 800x600. I should mention that i am using a prebuilt image with an edited boot.src due to issues with building android. also if anyone out there has a fresh virtual box (or vmware compatible) image i would greatly appreciate it if you could send me a download to it. Also i contacted the retailer/designers about this and they said it may be something to do with the sources relating/calling DDS if that means anything to you guys

Thanks in advanced!

Sandip