This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Why not use CLR instead of ABSSP?



This should be an easy question: Why not use CLR instead of ABSSP?

Say you want to get the absolute value of an SP floating point number.  You can do it two ways:

ABSSP     A10, A10                 ; This instruction imposes a Functional Unit Latency of 1.

CLR          A10, 31, 31, A10     ; This instruction effectively does the same thing, but without imposing any functional unit latency.

The CLR instruction operates here by zeroing the highest bit of the register, which is the sign bit of any single precision floating point number contained therein. Thereby producing its absolute value.

There is a minor difference between the two instructions, which may be negligible under many/most circumstances.  The difference is that the ABSSP instruction does some special handling for abnormal floating point numbers, such as setting flag bits as warnings.  (For example, if the original register contains something that is Not-A-Number (NAN), or denormalized, or infinity.) But those occur only under special circumstances (such as dividing by zero, etc.) 

If you are confident your original register contains a legitimate floating point number, then the CLR instruction will work to get the absolute value, and without the latency. Am I correct in this?

 

  • Walter,

    If you run simulations and get the exact same results for all the conditions that your program will encounter, you are certainly welcome to choose the assembly instruction that you prefer.

    Since you seem very familiar with SP binary formatting, you may be comfortable doing this.

    I would recommend other users to write their code in C and use the optimized output from the C compiler. If they wish to tweak it based on their similar understanding of SP formatting as yours, they might do the same. But I will not make any recommendation counter to how the compiler handles the operation. The compiler team knows the assembly instructions to a much finer detail than I do.

    Regards,
    RandyP