This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 PinMux question

Hi.

we need DM8168 to output to two video out port (one 24 bit => VOUT[0] and one 16bit => VOUT[1]). We need also two video inputs, the first at 24 bit (VIN[0]) and the second 16 bit (VIN[1]).

Using the PinMux tool it seems impossible to do that because VOUT[1] pins seems to be shared with most VIN[1] data pins.

Is this correct or I am missing something?

Thank you in advance.

  • Hi,

    Yes, This is correct, you can't use VOUT[1] and VIN[1] at same time because of pin mux constraints. But we have on-chip HDMI out for VOUT[1]. So you can use this. For any other format like VGA or YPbPr you need to use some kind of converter to convert from HDMI/DVI to VGA or something like that. 

    Regards,

    Hardik Shah