I have a new design in using a TPS65910AA1 and Sitara AM335X.
So far, the TPS65910AA1 does not fully come on. VRTC nicely ramps up with 1.8V. The 32 kHz oscillator looks fine. If a backup battery is connected it continues to run the oscillator. However, no additional rails come up. I am using the TPS65910AA1 is a failry dumb mode and not using it's power on/off, button or other features. I simply want the device to power and sequence up the AM335X when external power is applied. I am using boot 0b10 mode ( EEPROM ).
I am concerned I am in a "chicken and egg" scenario since the TPS65910AA1 supplies its own power to VDDIO and I have not had anyone confirm where the sequence state machine's power comes from, if it's from VDDIO or internal VRTC. I have looked through the SWCA139A TPS65910AA1 checklist and found no major discrepancies. I did miss connecting pin 30, VFB3 to ground, but I am not using SW3 related circuitry. I am concerned about the use of PWRHOLD, SLEEP and PWRON since I have no use for them but SWCA139A says I can leave them floating if not used.
I appreciate anyone's help.
- Cary