Other Parts Discussed in Thread: OMAP3530
Dear Experts,
Processor you are using: TI OMAP 3530
BSP version : 6.14.0
Platform (EVM or custom board): Custom board
Steps to reproduce the problem : how to compile camera module
I am tring to use OV9655 camera module on TI OMAP 3530 WinCE 6 BSP.
(OV9655 is a camera interace coms sensor) (OV9655 <--> OMAP3530 directly)
However, I have no idea how to achieve that ~
Two questions about TI OMAP Wince 6.14 BSP ~
1)-------------------------------------------------------------
I can see OV3640, but I don't know how to compile it ~
There are many environment variables in ti_evm_3530.bat.
Plz tell me how to set below environment variables:
set BSP_EVM2_VIDEO_CAPTURE=?
set SYSGEN_DSHOW_ERRORS=?
set SYSGEN_DSHOW_CAPTURE=?
set BSP_NOCAMERA_MDC=?
set SYSGEN_OSTEST=?
set BSP_NOCAMERA=?
set BSP_NOVRFB=?
or What environment variable or catalog should be set ??
How to compile it ~ in release mode or debug mode ??
Note:
a) I try to compile camera module with set BSP_NOCAMERA=NULL and add CAMERA in dirs, but it has many errors !
OV3640 camera module is failed in 6.14 BSP.
b) I have seen http://e2e.ti.com/support/embedded/wince/f/353/t/62997.aspx.
But I am not working on CAMERA_MDC model.
2) -------------------------------------------------------------
Does anyone can provide the driver to enable OV9655 CMOS Camera for TI OMAP3530 WinCE BSP?
-----------------------------------------------------------------------------------
3) Any camera application can use ?
-----------------------------------------------------------------------------------
OV9655 product brief http://www.ovt.com/download_document.php?type=sensor&sensorid=6
-----------------------------------------------------------------------------------
thx
HB