Hi,
I am trying to download the image file on to my AM387x/DM8148 EVM through ETHERNET,but i am not able to download the NK.BIN image file on to my EVM,could anyone help me out in resolving the issue.
These are the following steps i followed to download the OS design.
1) Enabled the KITL in BUILD options.
2) Commented all the NAND related functions(.dll).
3) Selected RAM BASED REGISTRY settings in catalog items.
4) Selected the local area networking devices to the appropriate.
5) Selected Clean SYSGEN command ,build was successful.
6) Connected the EVM and Host PC to the same subnet as the Host PC.
7) Inserted SD card,power on the EVM with SD boot switch settings, selected the boot device as INTERNAL EMAC from the menu.