TI document spra633c says the McBSP can be used in either the serial port mode or the general-prupose input/output mode. i want to know if McBSP can work in two of this mode at same time.
thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI document spra633c says the McBSP can be used in either the serial port mode or the general-prupose input/output mode. i want to know if McBSP can work in two of this mode at same time.
thanks.
i want to send messages from PC to DSK6416 through UART. and at same time i need to transport audio signal through McBSP. is this possible?
Yes. There are three McBSP ports on the C6416T. You can use them independently, so one can have its DR/DX pins connected logically to the PC and another can have its DR/DX pins connected logically to an audio device.
Regards,
RandyP
thank you very much. do i need any Peripheral added to the DSK to connect to the PC?
Please see the Application Note TMS320C620x/C642x McBSP: UART for a description of components needed to create this Hardware UART adapter interface to a DB9 connector.
Regards,
RandyP