This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LCD in U-boot for AM37xx boards

Hi all:

I'm trying to do support of lcd in u-boot for displaying a logo!

My steps what i have followed:

board.c

 stdio_init, drv_lcd_init, lcd_init ....

In config file, enabled CONFIG_LCD

our_logo.bmp added in tool/logos/Makefile

but while executing ,

i'm facing an error that is:

U-Boot 2010.06-rc1 (May 30 2012 - 12:20:58)

OMAP34xx/35xx-GP ES2.1, CPU-OPP2 L3-165MHz
OMAP3 Beagle board + LPDDR/NAND
I2C:   ready
DRAM:  256 MiB
NAND:  512 MiB
lcd_base = 80fb6000
omapdss_init
omapdss_init 1
value in control register = 00018309
omap_dss_init end
lcd_display_bitmap
Error: no valid bmp image at 80fb6000
In:    serial
Out:   serial
Err:   serial
Beagle unknown 0x01
Die ID #6e4600029e380000016830c501032014
Hit any key to stop autoboot:  0

But i'm not able to understand that bmp image address?

Please can anyone help me?

Regards,

santosh vastrad